Hungarian HEPENIX Ltd. is meeting entineering needs using the advantage of MISUMI products

 

Thanks to strong customer orientation of both HEPENIX and MISUMI, the two companies have main ‐ tained a successful business relationship over many years. HEPENIX uses MISUMI components in order to save time and costs without compromising the quality of its products.

 

Customer’s profile

HEPENIX Ltd. is a Hungarian company based in Diósd. The company which once was an engineering office has grown into a full ‐ scale machinery solution supplier ful ‐ filling the assembly, manufacturing and testing needs of its customers.

Since its foundation in 1991, HEPENIX has established itself as a reliable partner on the local and international market. HEPENIX provides the full range of services including the design, development, manufacturing, commissioning, and maintenance of special purpose machinery and is currently employing 35 engineers and technicians.

 

Initial Situation

In the early years of its existence, HEPENIX designed and manufactured nearly everything in‐house. With the growth of the company, a solution was due which would enable total cost savings for the company.In addition, it was important to focus on value adding technical processes for the customers.

HEPENIX and MISUMI first met at a trade fair where they started building a strong business relationship. MISUMI convinced the customer thanks to the reliability and availability of its products.

 

Measures

HEPENIX purchases MISUMI components on a regular basis. The customer is particularly satisfied with the quality of products and the wide product variety. The designers enjoy the vast number of possibilities MISUMI offers. They also appreciate the direct feedback of the Online Quote & Order System which notifies them directly in case of an incorrect product code. Another helpful feature of the MISUMI online system is the possibility to import bill of materials from tabulated format (e.g. MS Excel) so that information does not have to be typed in separately.

HEPENIX has also used MISUMI components in one of the most recent projects – a drive shaft press. Parts such as conveyor belts, covers, linear guides, rollers and cams were incorporated into the application.

Picture: a drive shaft press by Hepenix Ltd.

 

Result

By using MISUMI components, HEPENIX was able to concentrate on the overall design and could achieve sig ‐ nificant savings. In this way, they could cut down the design time by 10 – 15 per cent, according to the customer’s estimate.

“MISUMI understands our process – that we want to fulfil the needs of our customers – and is part of the solution.“ József Tóth, Director of Business Development

József Tóth, Director of Business Development

 

Benefit from MISUMI as well and become a customer!

Important information: Products of third-party suppliers (non MISUMI products) with a lead time of 4 days or less can be cancelled within 2 hours after order placement. Please refer to our cancellation policy and T&C for further details.