RAPiD Design(inCAD Components) Support

Frequently asked questions- About mates and constraints

4-10When mates and constraint components are edited in RAPiD Design(inCAD Components), are the mates and constraints transferred?

Mates and constraints may be transferred or not transferred depending on the component and what is edited.

Cases in which mates and constraints are transferred
  • Edits to the same model, such as changes to dimensions
    *Depending on the product, the model may be replaced, so in some cases mates and constraints are not transferred.
Cases in which mates and constraints are not transferred
  • When models are changed using the RAPiD Design(inCAD Components) function to change to a similar shape (click here for details)

Example: For a shaft support and shaft, if a T-shaped shaft support is replaced with an L-shaped shaft support while the shaft and shaft bore match, an error will occur on the feature tree

error

Back

Next