RAPiD Design(inCAD Components) Support

Frequently asked questions- About file saving

4-8How can I use the same component in a different size?

When a component imported from RAPiD Design(inCAD Components) is copied using SOLIDWORKS functions, it is recognized as the same component in RAPiD Design(inCAD Components). As a result, when the component size is changed, all components are changed.

When using the same component in different sizes, import all required elements from RAPiD Design(inCAD Components).
When saving from RAPiD Design(inCAD Components), you can save each file under a different name to ensure that each component is recognized as an independent component and changes can be made to its size without affecting other components.

A method for easily importing models with different dimensions is introduced here.

Back

Next