SOLUTION FOR BUFFER DRAWER
94% MISUMI products – even in complex applications
And the number of application areas is increasing every day. You can also configure and order from more than 20 million parts to save time and money when implementing your projects such as, for example, this puffer drawer for body-in-white production in automotive construction.
- Misumi Part
- Machined Part (predominantly of MISUMI raw material)
- Workpiece
The components, in this case the B-column panel, are placed in the intended component mounts in the open state of the buffer drawer. The exact position determination and locating of the components is ensured via guide brackets (NAAMS) and contour blocks/NC blocks (NAAMS). The reliable and trouble-free mount type protects the components against deformation and damage. Sensors detect the loading state and the correct positioning of the components. Manually cosing the drawer is assisted by dampers to prevent the components from being displaced. A pneumatic clamping device locks the drawer in the closed state during the picking process until the sensor system reports that the station has been unloaded. Only then will the pneumatic clamping device unlock and the drawer can be opened again so that the process can be started anew.
Discover the next station
Introducting our partner C-CON:
C-CON group has been looking ahead innovatively, courageously and on a global scale since 1991. We work with and for the automotive, aviation and aerospace industry, for their system partners and customers from the general mechanical engineering sector. We lead the way here, as we think ahead and outside the box. We are able to implement projects on a small scale or in their entirety and always act humanely, loyally and professionally.
Our Service
- Concept / complete vehicle
- Serial development
- Tool technology
- Mechanical processing
- Plant engineering
- Special machines and devices
- Plastic and lightweight construction production
- Project management
- Quality Management / Measurement Technology
- CAx method and process development / programming
- Trainingscenter