General Info

Intrinsic Vibration Behavior of Springs

In mechanical engineering, tension and compression springs are an important part of the design of mechanical systems, applications and uses. The properties of springs, such as their return force and spring constant, influence the performance and functionality of machines. In order to understand these properties and the vibration behavior of spring systems, we look in this article at the physical relationships between spring systems and the relationship between the natural frequency and resonance.

7 Minutes read

Turned parts – Precisely configurable Make-to-Order (MTO) components

Make-to-Order (MTO) turned parts and components are an important part of the modern manufacturing industry. Make-to-Order means contract manufacturing. This means that production only begins when a specific order is available. In contrast to Make-To-Stock (MTS), where products are produced for stock, MTO components are only manufactured after order receipt.

6 Minutes read

inCAD Library – A Designer’s Source of Inspiration

The inCAD Library is an extensive library for designers offering many application examples. The library provides freely application examples for functions or product possibilities. Each application example contains a parts list of the parts MISUMI has available together with information on the quantity required for the example. For designers, the CAD models serve as a source of inspiration for modifying, meaningfully adding and adapting them for their own machines or systems.

6 Minutes read

Mechanical Components for Automation Engineering

Automation engineering covers a wide range of components and technologies that work together to automate and optimize processes and machines. Mechanical components serve as one of the basic building blocks for the implementation of automated systems. These components include actuators, sensors, mechanical transmission systems and other mechanical elements required for the movement, control and monitoring of systems and machines. This article introduces the basics of automation and automation engineering and explains where mechanical components are used.

8 Minutes read

Measuring Technology – Quality Control Through Measuring Methods

In industrial manufacturing, measurement technology is a fundamental component for monitoring and quality control. Industrial measuring techniques allow collecting and quantifying precise data and information about the sizes, properties and characteristics of objects. The following article discusses the importance measurement technology has for quality assurance, and it introduces some methods from measurement technology.

8 Minutes read

Computerized Numerical Control – What is CNC actually?

Numerical controls, also known as NC controls, are devices for the targeted control of machines. They convert the coded data provided to the NC control on a data carrier into corresponding control commands and the resulting work and movement sequences. The introduction of the computer opened up new possibilities for improving NC controls and advancing them by integrating the computer into CNC controls. Both of these systems are examined in more detail in this article. In addition, it covers PLC control, which is also an approach to controlling machines and industrial equipment and is often used in combination with (C)NC controls.

9 Minutes read