Damping materials - Gel dampers
Whether in precision mechanical assemblies, automated equipment or the vibration isolation of sensitive components, gel dampers provide a highly effective, compact solution for energy absorption during motion, shock and vibration. This blog shows how mechanical damping works with gel, what the differences are from classic elastomer solutions, and what really matters when it comes to selection, installation, and material choice.
What are gel dampers and how do they work?
In many industrial applications, mechanical vibrations occur that must be controlled, limited, or completely eliminated. Without proper damping measures, movements often result in uncontrolled vibrations. If the system is excited into uncontrolled oscillation by vibrations, this can lead to malfunctions or damage. Gel dampers provide an effective solution in such cases: They specifically convert mechanical energy into heat, thereby creating a damped vibration in which the movement subsides in a controlled manner. This fundamentally differentiates them from purely elastic systems, which often cause rebound or resonance effects. Gel dampers operate quietly, precisely and reliably, even at the smallest amplitudes of motion or at high-frequency disturbances.
A gel damper uses a highly viscous gel, usually silicone-based, that is contained in a sealed housing to absorb energy. When a moving element, such as a shaft or a rotor, is moved through this gel, a flow-induced resistance is created. The resulting friction in the gel ensures that the kinetic energy is not returned but is dissipated as heat.
The result is a damped vibration: The amplitude of the movement decreases continuously without the system continuing to oscillate or spring back uncontrollably. The degree of damping can be specifically adjusted by means of the viscosity of the gel, the design of the damper and the speed of movement. As a result, gel dampers can be precisely adjusted to the desired damping behavior.
How do gel dampers differ from other damping elements?
Compared to classic rubber or PU rubber dampers, where the damping is due to the viscoelastic deformation of the material itself, the function of the gel damper is based on a fluid dynamic principle. Energy absorption here does not take place in the material, but in a medium - the gel - which is displaced or flowed through by mechanical motion.
Another difference lies in behavior under continuous load: While elastomers can fatigue and change shape over time, high-quality silicone gels remain largely resistant to aging. In addition, gel dampers do not require a restoring force. They provide purely damping action without springing, unless they are combined with a separate spring element.
What materials are used for gel dampers?
The performance of a gel damper depends significantly on the gel material used. This determines how strong, how uniformly and in what temperature range the damping takes place. In practice, three material groups are primarily used: Silicone gel, polyurethane gel and thermoplastic elastomer (TPE). They differ in their mechanical properties, their chemical stability and their processability - and thus also in the fields of application for which they are suitable.
Silicone gel
Silicone gels are the most commonly used materials in high-quality dampers, especially in applications where continuous loading, temperature stability or very gentle damping are required. They consist of polysiloxane-based chains that form a semi-solid, transparent gel through weak cross-linking. Silicone gels have the following characteristics in particular:
- Excellent thermal resistance, typical -40 °C to +200 °C
- very low glass transition temperature, which keeps them soft and damping even in the cold
- good aging resistance to environmental influences
- high dimensional stability without flow
Polyurethane gel
Polyurethane gels are based on the versatile polyurethane plastic system, which is converted into a gel-like, tough medium by controlled crosslinking. These gels are typically a little firmer than silicone gels, but offer significantly higher load-bearing capacity and abrasion resistance. Polyurethane gels have the following advantages:
- high tear and compressive strength
- adjustable viscosity and damping characteristics
- good adhesion to plastics and metals
- good chemical resistance, especially in ester-based systems
Thermoplastic Elastomer (TPE)
Thermoplastic elastomers, or TPE gels, combine the benefits of thermoplastics and elastomers. They consist of polymeric networks. They are dimensionally stable but can be processed thermoplastically. This makes them recyclable and particularly attractive for series production. These gels are known for:
- cost-effective manufacturing
- thermoplastically processable (no chemical curing)
- good haptics and malleability
- limited temperature resistance
Factors that influence the performance of gel dampers
The functioning of gel dampers is based on a fine-tuned interaction between material properties, geometry and movement parameters. In order for a gel damper to work reliably and efficiently in a specific application, various influencing variables must be considered, both in design and in operation.
Unlike classic elastomeric damping elements, which focus on material deformation, the damping effect of gel dampers depends heavily on the viscoelasticity of the gel, the speed of movement, the component geometry and the environmental conditions. Influences such as temperature, position of installation, material viscosity or the type of force induction directly affect the damping behavior and ultimately determine how well the system can absorb and control vibration, shock or movement.
Choice of material
The choice of gel directly affects the performance of a gel damper. Silicone gels offer particularly high thermal stability (typically -40 °C to +200 °C) and show little aging or hardening even under long-term stress. They maintain their damping effect consistently over many cycles and are also resistant to UV radiation and numerous chemicals. In addition, silicone gels protect against corrosive attacks, see our article on erosion and corrosion. Polyurethane gels, on the other hand, have higher mechanical load-bearing capacity and good processability, but are less heat resistant and more sensitive to moisture and aging. They are particularly suitable for applications with moderate temperature exposure and shorter life cycles.
Ambient temperature
The damping behavior of gel dampers is highly temperature dependent. As the temperature decreases, the viscosity of the gel increases - the damper becomes harder and responds more sluggishly. Conversely, viscosity decreases at higher temperatures, resulting in a softer damping effect. Silicone gels exhibit relatively stable behavior over a wide temperature range, while PU gels can be significantly more sensitive to temperature fluctuations. For applications with highly variable or extreme temperatures, silicone-based gels are usually the more robust choice.
| Material | Weather resistance | Water resistance | Oil resistance | Ozone resistance | Operating temperature range | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Silicone | ◎ | ◎ | △ | ◎ | -40 °C to +200 °C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Natural rubber | △ | △ | × | × | -30 °C to +60 °C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Chloroprene rubber | ◎ | △ | 〇 | 〇 | -20 °C to +70 °C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Geometry
The geometry of the gel body has a direct influence on the damping characteristics. Depending on the shape, thickness, and volume, the shear load that the gel is exposed to during movement changes. A thin gel gap produces higher shear forces and thus higher damping with the same movement, while larger volumes react more softly with less shear stress. By targeted adjustment of the geometry, the damping behavior can thus be fine-tuned, regardless of the material used.
Load Frequency
Frequency describes how many times a load—for example, a vibration or motion—repeats per second. Gel dampers are sensitive to this loading frequency because viscoelastic gels act differently at different frequencies. At low frequencies, the behavior of the gel is rather soft and fluid and produces a rather weak damping. As the frequency increases, the internal resistance of the gel increases, which significantly increases the damping effect. Therefore, it is essential to design gel dampers to exhibit the desired damping behavior in the respective frequency range—whether slow, dynamic, or high-frequency.
Aging and Fatigue
As with all materials, gel materials are subject to some aging and fatigue behavior, especially under thermal or chemical stress. Over time, the viscoelasticity or adhesion properties may change, which in turn affects the damping effect. Silicone gels usually show a high resistance to heat, UV, or oxidation. PU gels, on the other hand, are more sensitive and can harden, shrink, or become sticky with prolonged exposure to heat or moisture. Therefore, the planned service life and environment must also be taken into account in the design in order to avoid functional losses due to material degradation. To find out which test methods are suitable for this, please read our article on hardness levels and hardness tests.
Mounting Type
The type of installation also has a significant influence on the behavior of a gel damper. Depending on whether the damping element is pressed in, glued in, or freely supported, both the direction of action of the damping and the effective stiffness of the system change. With a fixed press-fit, the gel is additionally supported laterally, which can direct the damping more specifically in one direction and increase the stiffness. A free mounting, on the other hand, allows softer, more uniform damping in multiple axes. Bonding to certain surfaces also affects the sliding or adhesion behavior of the damper and thus its response to movement.
Areas of application for gel dampers
In mechanical engineering, gel dampers are used when classical elastomers meet their limits, e.g. during high-frequency vibrations, small movements or confined space.
A typical application is the vibration decoupling of sensitive assemblies, e.g. in measuring systems or optical devices, in which micro-vibrations can lead to loss of accuracy. In machine tools, gel dampers help reduce vibrations in the machining process, improving surface quality and reducing tool wear. Even with movable covers or panels, gel dampers ensure quiet, controlled closure without rebounding. This increases both comfort and durability. Last but not least, they serve as overrun brakes in linear guides to slow down end-of-line movements smoothly and vibration-free - ideal for automated operations with high repeatability.
Gel dampers are no longer used only as compact single elements. Increasingly, vibration-damping gels are also being structurally integrated into components in order to specifically dampen vibrations and decouple sensitive systems. Such applications can be found, for example, in gel vibration dampers, vibration damping gel bushings and vibration damping gel plates, which are used in a wide variety of industrial areas.
Gel vibration dampers typically consist of a housing with encapsulated, highly viscous gel, through which a moving element is passed. These dampers provide directional, speed-dependent damping and are ideal for small amplitudes and fine vibrations, e.g. in sensor brackets, fine mechanical axes or assemblies with high precision requirements.
Vibration damping gel bushings are an alternative to classic elastomer bushings, e.g. in the mounting of robot arms, small drive units or moving machine parts. Due to the gel structure within the bushing, the vibration energy is not only absorbed, but is specifically converted into heat via internal friction in the gel. This ensures a very quiet, uniform movement with a high decoupling effect at the same time.
Vibration-damping gel plates are often used as intermediate layers, base elements or supports, for example, for decoupling entire assemblies or devices. They can be designed in a variety of thicknesses and hardness levels and, especially in combination with rigid components, offer an effective way to reduce structure-borne noise and vibrations without complex geometries or fasteners. Low-microvibration support surfaces can increase the effect of gel plates.
Factors influencing the selection of the right gel damper
Gel dampers vary considerably in their material base, design, damping characteristics and durability. Depending on the operating environment, load profile and design specification, incorrect selection can significantly impair the desired damping effect or, in the worst case, lead to functional failures. In order to ensure reliable, durable and effective damping, the properties of the damper must be carefully adapted to the application scenario. The following outlines some of the key influencing factors that should be considered when designing a gel damper.
Type of load
Gel dampers can be designed specifically to either react strongly to sudden movements or maintain uniform damping over a long period of time. Gel viscosity, volume, and design are critical.
- For shock loads, such as closing flaps or intercepting moving parts, a gel with high viscosity and good energy absorption is required.
- For continuous loads, e.g. in lag brakes or guides, the gel must remain stable in the long term without deformation or hardening.
- With vibrations, in turn, especially in the micro range, fine, direction-independent damping is important – ideally with a low restoring force, as high-quality silicone gels offer.
Frequency range
The frequency at which a movement or vibration occurs significantly affects the damping effect. Depending on the application, the correct material type and geometry must therefore be selected in order to achieve the desired behavior.
- In high-frequency applications, such as those in electronics, fine mechanics or sensor technology, materials are required that reliably dissipate energy even in very small and fast movements without generating self-resonance.
- Low-frequency movements, such as typically occur in mechanical or plant engineering, require a gel that absorbs sufficient energy without reacting too softly or uncontrollably. Here, the geometry of the damper can also be adjusted in a targeted manner.
Installation environment
The installation situation largely determines which type of damper is suitable. Depending on the environment, the chemically and thermally suitable material must be selected.
- In confined spaces, compact or integrable damper solutions are required, such as a gel bushing or flat gel plate.
- Temperature requirements also play a major role: While PU gels usually remain stable up to approx. +100 °C, silicone gels can also be used at extreme temperatures between -40 °C and +200 °C.
- Chemical influences, such as oils, detergents, or moisture, require resistant materials.
Permissible residual movement or residual force transfer
In some applications, the damped component may still move back or spring back slightly after movement; in others, it should be stopped and held as completely as possible. Depending on the gel and the damper design, this behavior can be controlled.
- For safety-relevant applications or sensitive components, the most complete possible vibration isolation may be necessary.
- In other cases, some residual motion is permitted or even desired, for example, to gradually dissipate kinetic energy or obtain mechanical feedback.
Service life requirements
Depending on the application, a damper can go through several million cycles. The damping behavior must not decrease significantly.
- In high cycle-count applications, such as robotic axes, linear guides, or flap mechanisms, the gel must ensure high shape and damping stability over a long period of time.
- Silicone gels show particularly good aging resistance here and are suitable for applications with several million motion cycles.
- In less demanding applications (e.g., maintenance flaps or housing covers), a simpler PU gel can often be more economical and sufficient.
Current developments and innovations
New materials, modified design methods, and higher demands for precision, miniaturization, and sustainability are driving innovation. The focus is increasingly on tailor-made damping solutions that can be flexibly adapted to the respective environment and function. Five current lines of development are particularly in focus.
Nano-reinforced gels
An important trend is the integration of nanoparticles or nanoscale fillers into gel materials to significantly increase mechanical strength without losing their soft, damping properties. These nano-reinforced gels show improved rupture strength, dimensional stability, and temperature resistance, allowing them to be used reliably even in high-load applications or compact geometries.
Temperature-adaptive materials
Another key area of innovation focuses on temperature-adaptive gel materials, which automatically adjust their damping properties to the ambient temperature. These materials react to external influences such as heat or cold. This is intended to achieve a targeted change in viscosity, making them softer in cold conditions, firmer in warm conditions. The damping effect remains constant and reliable, even under highly variable operating conditions.
Miniaturization
With the increasing use of microelectronics, the need for ultra-compact damping solutions is growing. New micro gel dampers with edge lengths of only a few millimeters enable precise damping of very small motions or vibrations, including in sensor housings, miniature actuators, or folding mechanisms. This development opens up new possibilities in precision engineering and mobile electronics, where mechanical protection has so far been difficult to implement.
Recyclable TPE gels
As environmental compatibility requirements grow, recyclable gel materials based on thermoplastic elastomers (TPE) are being developed. These gels can be processed and recycled as thermoplastics without sacrificing essential damping properties. They offer an economical and environmentally friendly alternative to classic thermoset or silicone-based systems.
3D printing of gel structures
A particularly forward-looking approach is the additive manufacturing process (3D printing) of gel structures, which allows complex, application-specific geometries to be created with precisely defined damping behavior. For example, lattice structures, zones with graded hardness, or multilayer damping bodies can be manufactured directly from the gel material, without molds, without tool changes, and under full digital control. This opens up new paths in prototype development, small series production and individualization of damping elements.