Tutorial: Modulus of elasticity of steel – Materials science
Steel is an important material in modern industry and is used for a variety of applications. A crucial property to consider when using steels is their elasticity. The modulus of elasticity or Young’s modulus indicates how much stress is needed to achieve a certain degree of elongation. In this article we will look at the different types of steels and their respective elastic moduli.
What is steel?
Steel consists mainly of iron (Fe) and carbon (C), but other elements can also be added to improve or adapt its properties.
Most commercially available grades have a carbon content between 0.2% and 2%. The exact composition varies depending on the manufacturer and intended use of the material.
Today, thanks to modern technologies and research results, steel grades can be produced that have an impressive combination of properties. These properties are the result of targeted addition of alloy elements such as chromium, molybdenum or nickel in certain proportions.
The accompanying elements in steel also play an important role in determining its physical and chemical properties. Carbon, for example, increases the hardness of the material, while sulphur makes it brittle.
In addition, the crystal structure of the steel after deformation and its heat treatment condition are also decisive for its final mechanical and thermodynamic properties. Controlled cooling or heating processes can achieve a desired condition.
What grades of steel are there?
There is a wide range of different grades of steel, which are manufactured for different purposes. Some of the most common types are carbon steel, alloy steel and stainless steel.
Carbon steels have a high carbon content and are often used for construction elements such as beams or bridges. They can also be used in machine tools because they are hard enough to perform cuts. Due to their high strength and hardness, carbon steels are a popular material in special machine construction. They are particularly suitable for components that are subject to high loads, such as gear wheels or shafts.
In addition to iron, alloy steels also contain other elements such as chrome or molybdenum. These additives improve the strength of the material and its corrosion resistance to water or humidity. In special machine construction, alloy steels are used, for example, in the production of machine tool parts. In the production of special equipment for mining and tunnel construction as well as in the construction of cranes, alloy steels are also often used.
Rust-free (stainless) steels are characterised by their high resistance to rust - hence their name "rust-free". This makes it ideal for use outdoors and in environments with moisture exposure such as kitchen utensils or medical equipment. Rust-free steels and stainless steels are indispensable in special machine construction. They offer high corrosion resistance, which is especially beneficial in wet or aggressive environments.
In addition to these three main types, many other specialised steel grades are available on the market: High-temperature steels, for example, are used in extremely hot conditions; electrical steels, in turn, enable higher energy efficiency in electrical transformers; spring steels are used primarily in the construction of springs.
What is the modulus of elasticity for steel?
How is the modulus of elasticity determined for steel?
When elongated, the material undergoes the following phases:
- (1) - Elastic elongation, with straight lines by Hooke’s law
- (2) - Flow zone
- (3) - Solidification
- (4) - Constriction
- (5) - Breakage
The modulus of elasticity is defined by the linear range in the stress-strain diagram.
With uniaxial load in the tensile test, this linear range can be easily recognised: The higher the applied tensile force, the more the material expands - but always proportional to the force. The slope of this linear-elastic region then results in the modulus of elasticity of the material.
From this derivation, Hooke's Law applies with:
- E - Modulus of elasticity
- σ - Tensile stress
- ε - Strain
E-modulus of different steel types
It is important to note that the e-modulus not only depends on the chemical composition of the material, but is also influenced by the manufacturing process and the mechanical properties such as hardness or strength.
The higher the e-modulus of a particular grade of steel, the more robust the constructions made with it under load influences.
| Material | [N/mm2] |
|---|---|
| Structural steel (e.g. SS400/EN 1.0038 Equiv.) | approx. 210 x 103 |
| Mechanical steel (S50C/EN 1.1206 Equiv.) | approx. 210 x 103 |
| Pre-hardened steel (SCM440/EN 1.7225 Equiv.) | approx. 203 x 103 |
| Tool steel (SKD11/EN 1.2379 Equiv.) | approx. 210 x 103 |
| Brass | approx. 63 x 103 |
| Copper | approx. 105 x 103 |
| Aluminum (pure aluminum) | approx. 68 x 103 |
| Aluminum alloy (7xxx) "Duraluminium" | approx. 73 x 103 |