Product Info

Belt conveyors – Construction, conveying capacity and belt selection for optimized processes

Belt conveyors are versatile conveyor systems that play a critical role for optimizing industrial production processes. From its basic design to the various types of drives to the capacity of the conveyor, this blog highlights how to get the most out of your conveyor. We will also take a look at the different belt shapes used on belt conveyors and will show you what to look for when replacing the belts to ensure smooth operation in your industrial plant.

7 Minutes read

Rollers and wheels for industrial uses – Construction and applications

In mechanical engineering and in general automation processes, it is essential that materials and construction components are transported quickly and efficiently from A to B. This requires purposeful guidance and alignment along the conveying paths. Rollers and also drums contribute significantly toward fulfilling these functions. This article examines which types of materials are used and for which specific applications rollers are used.

12 Minutes read

Details of elastomer inserts for couplings

Elastomer couplings are a type of shaft coupling. They transfer torque between two shafts and perform tasks such as power transmission, compensating alignment errors, but also damping of shocks and vibrations. Elastomer couplings ensure optimal power transmission by using various materials, and also based on their material properties and shape. The properties of the respective elastomer coupling simultaneously prevent vibrations of the drive shaft from being transmitted to the coupled shaft. The following article discusses which properties these are, how the hardness of elastomers is determined and what application examples there are.

7 Minutes read

Worm Gear – Low-Noise Gear Ratio Expert

Worm gears are an important part of the design of many machines and systems. They offer high gear ratios and torque transmission, while taking up only little space in mechanical application thanks to their space-saving design. In order to find the best possible solution for your specific requirements, it is important to select the right components based on the required specifications and performance requirements.

7 Minutes read

Positioning Stages as Optimal Guide in the Machine – Overview and applications

This article explores the different types of manual stages and their applications. Manual stages are special tables that are used, among other things, in quality assurance and automated measuring technology for calibration and process monitoring.

5 Minutes read

Cantilever pins/cantilever bearing pins – Design and application

Cantilever pins/cantilever bearing pins are essential fasteners that are used in numerous mechanical systems to store and connect rotating components. They act as pivoting points and contribute to the stability and precision in applications in mechanical engineering and automation. This article introduces various designs and examples of applications of cantilever pins and cantilever bearing pins.

7 Minutes read