Drill Bushings - Benefits/Types/Application/Overview of Standards

Drill bushings are an important part of machining workpieces. They are used to guide the boring tool safely and precisely, thus ensuring an exact bore. This article details the benefits, types, applications, and standard overviews of drill bushings.

What are drill bushings and what are they used for?

Drill bushings, also called positioning bushings, are cylindrical components that are used daily, especially in mechanical engineering and vehicle construction. They facilitate accurate hole with tight tolerance and precise location positioning.

In principle, drill bushings act as a guide sleeve during drilling operations. They are therefore used to guide the drill bit in the drill fixture so that the drill bit can run stable and straight.

This is of enormous importance, for example, on so-called deep drilling, since significant forces act in this method, which can cause the drill to slip or slide. The use of drill bushings eliminates such risks and provides precise and dimensionally accurate drilling without wandering or tearing.

Drill bushings are also called positioning bushings or centering bushings, as centering pins or support pins can be positioned over the rounded opening of the drill bushing.

Drill bushing applications

Cylindrical Drill Bushing Collar Drill Bushing Socket Drill Bushing
Cylindrical drill bushings are usually countersunk flush into the bore of a workpiece. Then, they can be mounted with the component. Collar drill bushings are countersunk up to the stop of the collar. They can again be disassembled. Socket drill bushings have a stop similar to the collar drill bushings. They are designed to ensure that the drill bushing can be replaced as quickly and easily as possible.
Cylindrical drill bushings are used in fixtures that are not under a heavy load, e.g. guides for pins or drill guides in soft materials. Collar drill bushings are easier to mount and when subjected to axial forces, the collar acts as a stop, reliably preventing the drill bushing from sliding into the bore. Socket drill bushings are also easy to mount, but even easier to remove because the stop pins are removed and the knurled surface makes the bushing easier to grip and therefore remove.

What are the benefits of drill bushings?

Drill bushings are standardized parts with enormous variety and offer numerous advantages. Compared to hand-held drilling, the drilling process is simplified and improved, greatly optimizing industrial drilling processes.

  • Repeatability: The use of drill bushings allows for quick drilling because the tool positioning is always the same due to the bushing. Consequently, the drill points do not need to be remeasured after each bore.
  • Precision: The use of an appropriate bushing provides high drilling accuracy. The drilling process can in turn be optimized by means of a dimensionally accurate drilling pattern.
  • Consistent quality: The drill holes have a consistent result due to the use of drill bushings and thus are of the same quality. This is especially important in mass production.
  • Protection against damage: Drill bushings prevent the drill bit from wandering. The workpiece is protected by the bushing so that there are no scratches or damage to the surface.
  • Low wear: A suitable bushing reduces wear on the inserted tool.

What are the types of drill bushings?

Drill bushings are highly varied. Depending on the requirement and application, there are three different versions.

  • Cylindrical drill bushings iaw. DIN 179
  • Collar drill bushings iaw. DIN 172
  • Socket drill bushings iaw. DIN 173

Cylindrical drill bushings iaw. DIN 179

Cylindrical drill bushings are used in many industrial applications. They are often used as guide elements for tools or machine parts and are characterized by their high precision and robustness.

The special features of cylindrical drill bushings include their cylindrical shape and the fact that they do not have a bump stop edge. Due to the missing bump stop edge, these types of drill bushings have the same inner diameter and outer diameter throughout.

Particularly o softer materials, such as plastics, cylindrical drill bushings can be pressed in accurately and with a precise fit to provide a highly accurate drilling result.

Collar drill bushings iaw. DIN 172

Collar drill bushings are another special type of drill bushing widely used in industry. They are often used as guide elements or bearings and are particularly characterized by their high precision and load-bearing capacity.

As the name suggests, these types of drill bushings have a collar on one end. This circumferential collar prevents the drill bushing from being pushed through the seat of the drilling device when machining the workpiece. Due to their design, collar drill bushings have two different outer diameters.

Socket drill bushings iaw. DIN 173

Similar to collar drill bushings, socket drill bushings have two different outer diameters. At their larger outer diameter, socket drill bushings are often equipped with knurling for optimized grip. In addition, these variants have a round segment or notch on the larger outer diameter. This allows the bushings to be secured to prevent the bushing from twisting during drilling.

Compared to cylindrical drill bushings, socket drill bushings have the advantage of being easy and quick to replace. Different diameters can therefore be drilled in a short time by replacing the socket drill bushing.

The use of different types of bushings ensures a precise fit into the drill fixture or workpiece, which also leads to a higher quality of the end product.

Key parameters for selecting drill bushings

There are many factors and characteristics to consider when selecting the correct drill bushing. In addition to the inner diameter and outer diameter, other factors such as material and hardness must be taken into account, but also the type of rounding and fastening method.

The right drill bushing is key to avoiding inaccurate, defective bores and to achieving clean, precise results.

Bore rounding - Shape A and Shape B

Collar drill bushings and cylindrical drill bushings are differentiated into two different shapes: shape A and shape B. The distinguishing feature is the embodiment of the bore.

The bore is rounded at one end on shape A drill bushings. By contrast, shape B bushings have the holes rounded on both ends.

The figure clearly shows the difference between the two shapes A and B. While shape A has the bore rounded on one end, shape B has the bore rounded on both ends.

Shape B is designed to be used from both sides. The rounded sides reduce stress peaks and improve service life. By contrast, shape A can be completely guided through the fit to the exit of the bore, this providing greater precision.

The shape is selected according to the specific use cases.

What to consider when selecting the right size?

When selecting cylindrical drill bushings, it is extremely important to ensure that the size of the drill bushing perfectly matches the drill bit.

A bushing that is too small will prevent the drill from being inserted properly, resulting in unclean or even seized motion. On the other hand, the clearance between the drill and the bushing must not be too large, as this would make proper tool guidance impossible.

The ideal spacing limit for drill bushings is in the range of 0.01 to 0.03 mm. This optimizes tool guidance and achieves accurate results.

What materials are drill bushings made of?

Drill bushings are often made of so-called case-hardened steel. Case-hardened steel is unalloyed or low-alloy structural steel characterized by very low carbon content. The advantage of this material is the high edge hardness, which in turn ensures optimum wear resistance of the surface.

However, a high edge hardness also has some disadvantages, especially if drill bushings made of steel are used in combination with centering pins as centering bushings. This can damage the pin tips due to friction forces and wear on the bushings due to the high loads.

To solve these problems, new technologies have been developed – so-called “low-impact” or “gentle” types of positioning bushings. These are specifically designed to avoid damaging the pin tips during the alignment process while ensuring precise placement.

In particular, brass drill bushings are very gentle and prevent the centering pins from wearing out excessively quickly. Gentle brass drill bushings are available in MISUMI’s extensive range.

Why MISUMI drill bushings?

All drill bushing versions have their advantages and disadvantages, depending on the application. In addition to the technical properties, factors such as ambient temperature and possible dirt or moisture influences at the job site are important when selecting a suitable drill sleeve.

High-quality MISUMI drill bushings should therefore be used to benefit from longer machine service life and higher productivity based on more accurate results in the machining process.

MISUMI offers a wide range of drill bushings of all kinds to meet the vast range of requirements. Our drill bushings are manufactured according to the latest production processes and are of the highest quality to guarantee safe use.

Our shop lets you choose between the versions of drill bushings:

MISUMI also has other machine components that can be used for fixture construction, for example: