Specialty plastics for practitioners – Properties, resistance and application examples

Specialty plastics are used when applications place high demands on the material or special properties are required. They frequently have insulating properties and their high resistance to water and chemicals makes them a reliable, low-maintenance material. It is then no wonder that specialty plastics are used in many technical fields and also in fasteners such as screws and nuts. The following article provides an overview of various specialty plastics and their applications.

What are specialty plastics?

Specialty plastics are designed to meet requirements that ordinary plastics cannot meet. The special properties are for example achieved by modifying the chemical composition or by special-purpose manufacturing processes. Specialty plastics, or high-performance plastics, are often specialized in terms of one property.

Manufacturing process for specialty plastics

When producing specialty plastics, the material composition is important to achieve the ultimately desired properties. The following example describes the production of PTFE:

Production process using PTFE as an example

Polytetrafluoroethylene, or PTFE, is made of chlorinated hydrocarbon. It can be produced by two methods, which differ depending on the desired starting product (powder or dispersion). Fluorides are partially added to the chlorinated hydrocarbon, which initially generates the gasses chlorine difluoromethane and tetrafluoroethylene. The tetrafluoroethylene is then dissolved in an aqueous phase, while excluding oxygen and exerting high pressure, and is then polymerized to PTFE by adding an aqueous initiator solution. Because PTFE is not water soluble, it precipitates in the aqueous phase. The PTFE is then obtained in the form of a powder by filtration and drying. If a dispersion is to be obtained as the starting product, a dispersant is added to the aqueous solution before the addition of the initiator.

Types of Specialty Plastics

There are a number of plastics that are suitable for producing components for specialized applications, such as plastic screws. At MISUMI, we offer a wide range of components made of the following plastics:

Overview of various specialty plastics
Short name Name Microstructure Classification Description
ABS Acrylnitrile butadiene styrene amorphous Standard plastics High resistance to mechanical stress, very hard
Bakelite Phenoplasts based on phenol and formaldehyde Duroplast Engineering Plastics Bakelite plates from MISUMI are suitable as insulation plates for electrical panels, control units and breakers. The paper-based version is available in natural color and black, a stronger fabric-based version is also available. The Bakelite color (natural color) can vary by production batch. However, this does not affect the quality.
ETFE Ethylene-Tetrafluoroethylene-Copolymer Semi-crystalline High-performance plastics Fluorinated co-polymer made of tetrafluoroethylene and ethylene. Has very good properties against mechanical wear, electrically insulating, chemically very resistant, suitable for use in high temperature applications.
FEP Fluoroethylene propylene Semi-crystalline High-performance plastics Polymer, also known as TEFLON (fluoropolymers group), excellent chemical corrosion resistance, excellent temperature resistance, is often used as sealing and filling material, FEP has a greater coefficient of friction and a lower continuous operating temperature than PTFE.
MC nylon Name for a group of long-chain polymer amides (PA) / nylon Semi-crystalline Engineering Plastics Monomer casting. With better abrasion resistance than POM, it is generally used for linear guide plates. MISUMI manufactures three different gliding categories: Gliding category with greatly improved gliding performance, high-strength category with excellent strength and conductivity category for use around electrical components that require electrostatic protection. A category with good weather resistance that protects against heavy wear is also available. General properties: ductility, strength, abrasion and fatigue resistance, low friction coefficient.
PA 12 Polyamide 12 / nylon 12 Semi-crystalline Engineering Plastics Typical properties of nylon: high ductility, high temperature resistance, high water absorption (softener), good wear resistance, resistant to many oils, greases and fuels, good gliding and friction properties, high impact strength, used in motor vehicles and aircraft for fuel, hydraulic lines, etc.
PA6 Polyamide 6 / nylon 6 Semi-crystalline Engineering Plastics Typical properties of nylon: high ductility, high temperature resistance, high water absorption (softener), good wear resistance, resistant to organic solvents, good gliding and friction properties, high impact strength, high mechanical damping properties
PBT Polybutylene terephthalate Semi-crystalline Engineering Plastics High abrasion resistance, high impact strength, strength and stiffness slightly lower than PET, very good gliding and wear properties, good electrically insulator, chemical resistance comparable to PET, used for gliding and roller bearings, screws, connector strips, parts of household appliances
PC Polycarbonate amorphous Engineering Plastics Highest impact resistance among transparent plastics (approx. 30 times higher than PMMA), excellent temperature resistance and extensive range of uses.
PE Polyethylene Semi-crystalline Engineering Plastics Good electrical insulator, high ductility, good gliding behavior, low hardness and strength, low wear, good resistance to many acids, bases, greases and oils. Density as differentiating feature. In PE-LD and PE-HD with slightly different properties (LD is softer, more flexible and more shatterproof, but less resistant to abrasion than HD) - applications: Household goods, storage containers, transport boxes, vehicle tanks, etc.
PEEK Polyetherether ether ketone Semi-crystalline High-performance plastics PEEK is a very good, high-performance semi-crystalline engineering plastic. It has the highest chemical resistance among technical plastics. PEEK can only be dissolved in concentrated sulfuric acid. It has excellent heat resistance, abrasion resistance, flame resistance and hydrolysis resistance.
PET Polyethelium terephthalate Amorphous or semicrystalline Engineering Plastics approx. 4 times higher impact resistance than PMMA, environmentally friendly material that does not release toxic gases during combustion and is cost-effective.
PE-UHMW
(also: UHMW-PE)
UHMW polyethylene Semi-crystalline Standard plastics UHMW polyethylene with extremely high molecular weight. Has very good abrasion and wear resistance, high chemical resistance to chemicals, good gliding properties, self-lubricating and is very shock-resistant.
PFA Perfluoroalkoxy Semi-crystalline High-performance plastics Polymer also known as TEFLON (group of fluoropolymers). It combines the chemical properties of PTFE with the mechanical-technical properties of FEP. PFA is resistant to chemicals, temperature-resistant, UV radiation-resistant, and excellent electrical insulator and extremely weather-resistant.
PI Polyimide amorphous High-performance plastics Non-meltable, excellent temperature resistance, high mechanical strength, high shape stability, very good friction and wear properties.
PMMA Polymethyl methacrylate amorphous High-performance plastics Also known as acrylic glass or the brand name Plexiglas. It has excellent transparency, weather resistance and machineability, medium strength, high rigidity, is relatively brittle, has good electrical insulation properties, polishing properties, resistant to acids and alkaline solutions of medium concentrations.
POM Polyacetal Semi-crystalline Engineering Plastics Excellent mechanical strength; used as a material in many cases for wheels, rollers and gear wheels.
PP Polypropylene Semi-crystalline Standard plastics High strength and hardness, good chemical resistance to many acids, bases and solvents, good insulator, used in the food industry, but also furniture, automobiles and chemical-pharmaceutical industry.
PPS Polyphenylene sulfide Semi-crystalline High-performance plastics PPS is an excellent crystalline engineering plastic. It has excellent heat resistance, and the physical properties are not impaired even during extended use at high temperatures. It also has excellent chemical resistance, mechanical and electrical characteristics, and is dimensionally stable.
PPS / HPV PPS Fiber-reinforced polyphenylene sulfide type   Engineering Plastics Techtron® HPVPPS is a product based on the superior heat and chemical-resistant PPS and has significantly improved gliding properties. Used in high-temperature gliding components with high PV values.
PTFE and PTFE (F4) Polytetrafluoroethylene Semi-crystalline High-performance plastics Polymer also known as TEFLON (group of fluoropolymers). Has excellent chemical corrosion resistance, excellent temperature resistance, is often used as sealing and filler material. PTFE has a lower coefficient of friction (currently regarded as the smoothest material available) and a higher continuous operating temperature than FEP.
PVC Polyvinyl chloride Semi-crystalline Standard plastics Resistant to acids, alkaline solutions, alcohol, oil and gasoline, flame retardant, low thermal conductivity, very good insulator against electricity, light and sound.
PVDF Polyvinylidene fluoride Semi-crystalline High-performance plastics Resistant to a variety of chemicals, high mechanical strength, high UV and weather resistance, high temperature resistance, applications: Apparatus construction, packaging, food and pharmaceutical industry, electrical devices of all kinds, tubes, glide bars, screws, etc.
RENY Glass-fiber reinforced polyamide MXD6 nylon crystalline Engineering Plastics RENY is based on the MXD6 polyamide and crystalline engineering plastic reinforced with 50% glass fibers. It has the highest strength and elasticity in plastics and also exhibits very good oil and heat stability. It can therefore be used as an alternative to metal.
High performance Technical Standard PPS, PEK, PEEK, ETFE, FEP, PVDF PI, PMMA PCM, PA6, PA 66, MC Nylon PA 11/12, PBT, PE, PET PC, PMMA PP, PE-HD, PE-LD, PE-LLD, PVC ABS, PS, PS-HI Semi-crystalline g isolation="isolate"> amorphous Price and performance Production volume

Advantages and disadvantages of plastic

Plastic connecting elements have the following advantages:

  • They usually have an insulating effect, both thermally and electrically.
  • They often expand similarly to natural materials.
  • They are often resistant to water and many chemicals.

When compared to metal fasteners, their disadvantages are that they often have lower resistance to tensile and compressive forces, as well as lower maximum application temperature. This should be taken into account, for example, when selecting plastic washers.

Chemical resistance of selected plastics

The following table provides an overview of the chemical resistance of selected plastics:

Chemical resistance of selected plastics
  PC PPS RENY PEEK PVC PP PTFE PFA PVDF Ceramic POM PA6 PA66 PA12
  Acids                          
Hydrochloric acid 10% o o x o o o o o o o x x x x
Sulfuric acid 10% o o x o o o o o o o x x x ^
Sulfuric acid 50% ^ x x x x - o o o ^ x x x x
Nitric acid 10% o o x o o o o o o ^ x x x x
Nitric acid 50% ^ x x x x - o o o ^ x x x x
Hydrofluoric acid 10% o ^ x - - o o o o x x x x -
Hydrofluoric acid 50% ^ x x x - ^ o o ^ x x x x -
Phosphoric acid o ^ x o o o o o o x x x x ^
Formic acid o o x ^ ^ o o o o - x x x x
Acetic acid o o x o ^ o o o o - ^ x x ^
Citric acid o o ^ o o o o o o - ^ ^ ^ ^
Chromic acid o ^ x o o o o ^ o ^ - ^ - ^
Boric acid o o ^ o o o o ^ o ^ - ^ - o
  Alcohols                          
Methanol ^ o - o o - o o o o o - - ^
Butanol - - - o - - - - o - o - - -
Glycol o o - o - - o o - o o - - o
  Aldehydes and ketones                          
Acetaldehyde x - o o - o o o o o o - - ^
Acetone x o - o - - - - - - - - - -
Formaline - - - o - - - - - - - - - -
Methyl ethyl ketone - - - o - - - - - - - - - -
  Alkali                          
Ammonia x o o o o o o o o - x o o o
Sodium hydroxide 10% - o o o o o o o o - ^ o o o
Potassium hydroxide 10% x ^ o o o o o o o - ^ o o o
Calcium hydroxide o ^ x o o o o o o - o x x o
  Halogenated organic substances                          
Tetrachloride carbon - - - o - - - - o - - - - -
Perchloroethylene - - - o - - - - o - - - - -
Freon 12 - - - o - - - - - - - - - -
  Hydrocarbons                          
Benzene x - - o - - - - o - - - - -
Toluene x o - o - - - - o - - - - -
Xylol - - - o - - - - - - - - - -
Cyclohexane - - - o - - - - ^ - - - - -
Napthalene - - - o - - - - - - - - - -
  Inorganic chemicals                          
Water o o o o o o o o o o o ^ ^ o
Hydrogen sulfide o o o o - o o o o - ^ o o o
Sulfur dioxide - ^ o o - o o o - - o o o -
Sodium chloride o - o o - o o - o - o o o -
Ammonium salpeter x o o o - o o o o - ^ o o -
Sodium nitrate - o o o - o o o o - ^ o o o
Sodium acetate x - o o - o o - o - o o o -
Calcium carbonate o o o o - o o o o - o o o -
Calcium chloride o o o o - o o o o - o o o o
Magnesium chloride o o o o o o o o o - o o o -
Magnesium sulfate o o o o o o o o o - o o o -
Zinc sulfate o o o o - o o o o - ^ o o o
Hydrogen peroxide o ^ ^ o o o o o o - x ^ ^ ^
  Chemicals                          
Urea o - - o - o - - - - ^ - - -
Detergent o - o o - o - - - - o o o -
o = can be used
^ = can be used under certain circumstances
x = cannot be used
- = no data

Application example: Plastic sleeves and plastic washers

Spacer sleeves are used in many designs to create a distance between two components. They are cylindrical and can for example consist of rubber, metal or plastic. The purpose can be to insulate, reduce friction, or control movement. Plastic spacer sleeves offer several advantages over metallic spacer sleeves: They are insulating (thermally or electrically depending on the material) and are similar in properties to natural materials. Plastic sleeves expand, for example, to a similar extent as wood and other soft materials.

The insulating properties make plastic sleeves the ideal component in electrical engineering, e.g. for securing electronic components on a printed circuit board or for correct alignment and for maintaining safe distances between components. Spacer sleeves are also often used in mechanical engineering to accurately hold components in position or to dampen vibrations and noises. Another option would be as a bearing sleeve or mounting aid for light components.

  • 1 - Plastic sleeve with guide
  • 2 - Rotary shaft
  • 3 - Timing pulley
  • 4 - Ball bearing
  • 5 - Bearing housing with bearing
  • 6 - Drive wheel

If plastic discs are to be used that need to be conductive, MISUMI offers conductive and antistatic versions made of MC nylon in addition to standardized versions.

Various plastics are also used in washers. Here too, thermal and electrical insulation is the key criterion for their use. MISUMI for example also offers plastic discs with gliding properties. Discs and sleeves made of fluoroplastics for example reduce friction resistance in hinge designs. Due to their excellent thermal insulating properties (melting point is up to 300°C, depending on the strength and composition), Polyether Ether Ketone (PEEK) discs can in turn be used in heating and cooling lines.