Pneumatics - Calculating air consumption and required air volume for pneumatic cylinders

How much compressed air does a pneumatic cylinder really need? In this article, you'll learn how to calculate the air consumption of double-acting cylinders and which influencing factors are critical. In industrial applications of pneumatic systems, precise analysis of air demand is essential to conserve energy and increase plant efficiency. In practical terms, we show what matters in the calculation, including the formula, an example, and tips for optimization.

Fundamentals of Pneumatics

In pneumatics, air or another neutral gas is used to perform mechanical work. Unlike in hydraulics, where fluids are used for power transmission, a gas serves as a fluid in pneumatics.

But how exactly does pneumatics work?

Compressed air is generated by compressors that draw in ambient air, compress it to up to 40 bar, and feed it via storage tanks or directly into pneumatic drives as needed. Careful conditioning of compressed air using filters is essential to remove contaminants such as dust, water, or oil and to ensure the operational reliability of the systems. Finally, the compressed air is supplied to the respective machine components via a suited pipe network, where it is used to generate motion (mechanical work).

Pneumatic cylinders in operation
Pneumatic cylinders in operation

The air provided for pneumatic applications must be extensively conditioned and compressed. This is sometimes associated with high costs. Unlike hydraulically operated systems, air-operated equipment leaks tend to have no environmental impact, but can cause high supply and conditioning costs for the operating fluid. Leaks should therefore be avoided and corrected as soon as possible. Nevertheless, the air provided for operation should be able to provide the calculated air requirement of the application plus a reserve for leaks and for pressure losses and pressure fluctuations occurring in the system. For the optimal sizing of the conditioning system and compressed air containers, the air requirement of the components (loads) used must be calculated, see also the separate section.

There are many advantages to using pneumatic components:

  • Compressed air is easily stored in compressed air containers.
  • The application is particularly clean because there is no liquid to leak.
  • Using compressed air minimizes the total weight of a plant or machine.

However, there are also disadvantages when using pneumatics. A comparatively large amount of noise and cold is produced. Maximum piston force is based on operating pressure. This is limited by the effort required for conditioning and storage. In addition, the air usually carries an oil mist. This can settle in the event of leaks in the surrounding area or lead to contamination when blowing off components.

Basics of Pneumatic Cylinders

Pneumatic cylinders convert compressed air into linear motion used for a wide range of applications. There are two basic types: Single-acting and double-acting cylinders.

Single-acting cylinders have a single air connection, while a spring or external load retracts them. They feature simple construction and compact dimensions.

Double-acting cylinders use compressed air for both directions of motion. They have two compressed air connections. Since the piston of a double-acting pneumatic cylinder is also retracted by compressed air, they have a higher compressed air requirement than single-acting pneumatic cylinders.

Calculating compressed air consumption

The supply and conditioning of compressed air cause ongoing operating costs. It is recommended to calculate the compressed air consumption because this forms the basis for selecting optimally sized compressors and conditioning systems. The goal is to avoid under- or over-sizing while ensuring efficiency and operational safety.

In addition, monitoring, such as monitoring specific performance (efficiency), leakage rate and occurring pressure losses, can continuously optimize the system and control maintenance measures in a purposeful manner. Modern online tools and calculators help you calculate compressed air costs quickly and accurately. Standardized symbols in the pneumatic circuit diagram, such as the symbol for air consumption, are also helpful and provide a quick overview of the air demand points of a system in technical drawings and plans.

The air consumption Q of a double-acting cylinder depends on piston diameter, stroke, operating pressure and cycle frequency. The conversion to standard liters is carried out taking into account the pressure and the environmental conditions.

The following formula can be used to calculate compressed air consumption. The mean air pressure of the atmosphere Pamb (1013.25 hPa = 0.1013 MPa) is usually used for the calculations.

Compressed air consumption of single-acting cylinders

Q = A_1 \times s \times n \times\frac{p_{e}+p_{amb}}{p_{amb}}
A_1 = \frac{\pi \times d^{2}}{4}

 

• Q = compressed air consumption per minute in cm3
• A1 = piston area in cm3
• s = piston travel in cm
• n = number of strokes per minute
• d = piston diameter in cm
• Pamb = standard air pressure
• Pe = overpressure above Pamb

Compressed air consumption of double-acting cylinders

Q = (A_1+A_2) \times s \times n \times\frac{p_{e}+p_{amb}}{p_{amb}}
A_1 = \frac{\pi \times d^{2}}{4}
A_2 = \frac{\pi \times (d_1^{2}-d_2^{2})}{4}

 

 

• Q = compressed air consumption per minute in cm3
• A1 = piston area in cm3
• A2 = piston rear surface in cm3
• s = piston stroke in cm
• n = number of strokes per minute
• d1 = piston diameter in cm
• d2 = piston rod diameter in cm
• Pamb = standard air pressure
• Pe = overpressure above Pamb

Optimizing compressed air consumption

Air compressors have high energy consumption, and compressed air should be used as efficiently as possible to avoid unnecessary costs. By calculating compressed air consumption, you have already taken a first step towards optimization. Another approach to increasing efficiency is to analyze and minimize the factors influencing compressed air consumption. Leaks are a major problem. On average, up to 30% of compressor capacity is lost through leaks, especially in poorly maintained compressed air systems. These losses force compressors to continuously deliver higher pressures, significantly increasing energy consumption per air volume produced. In addition, leaks cause unstable pressure conditions, result in unplanned downtime, and increase operating costs due to frequent maintenance and unplanned outages. Unlike hydraulic systems, where leaks are easily detectable by escaping fluid, locating the leak in pneumatic systems is more difficult. For example, regular use of ultrasonic measuring devices is recommended. Using a leak detection spray can also help make leaks in the system visible. Minor leaks are indicated by the leak detection spray by foaming. Weak points in the system are often: threaded connections, connection points, hoses, pneumatic valves, or regulators. Flow meters can also be used to ensure in the long term that leaks are detected and corrected quickly.

Another option to optimize compressed air consumption is the purposeful use of air filters, pneumatic valves, or regulators. At MISUMI, you will find a wide range of options in the webshop, e.g. pneumatic filters and pneumatic pressure valves.

MSAF air filter
MSAF air filter

Compressed air tanks support the storage of generated compressed air. They act as a buffer, stabilize system pressure, and balance air demand fluctuations, thus avoiding sudden pressure spikes and increasing system service life. By buffering compressed air, the compressor can operate more uniformly and in a more efficient load range, significantly reducing both energy consumption and wear. In addition, properly sized containers allow for flexible adaptation to load changes and integrate seamlessly with modern energy management systems to optimize overall energy usage.

Common errors when selecting pneumatic cylinders

When selecting pneumatic cylinders, preventable errors are common, which can affect the performance, reliability, and efficiency of the overall system. One of the key errors is insufficient consideration of application-specific factors such as load mass, stroke length, or operating environment, which can lead to malfunction, premature wear, or poor performance. Undersizing and the resulting insufficient piston force are also critical. It can cause the cylinder to stall under load or operate too slowly, thus compromising process efficiency and cycle times. Equally important is the correct calculation of the actuation speed to avoid production delays. For more information on choosing a pneumatic cylinder, see our article about selecting a compact compressed air cylinder in 6 steps.

Another common mistake is neglecting air supply and actual air consumption. If there are bottlenecks or pressure drops, operation can become unstable or even fail completely at peak load. Improperly sized supply lines, valves, pressure regulators, cylinders, or incorrectly designed flow restrictors often result in unnecessary energy consumption or insufficient compressed air supply.

In addition, environmental factors such as temperature, corrosion exposure, or cleanliness requirements play a critical role in material selection. For example, if end-position cushioning is not taken into account, mechanical damage can be caused by hard stops, resulting in high costs and downtime in the long run. Always ensure the supply of dry and clean air by using a filter and dryer. Contamination in compressed air can cause malfunction or damage.