Profile connectors for aluminum construction profiles - Accessories

Precisely matched profile connectors are essential for the efficient construction of machine frames, guards and workstation systems. MISUMI’s webshop offers an extensive range of connecting elements that covers various mechanical requirements and profile geometries. What solutions are there and how can they be implemented? In this article, we provide a structured overview of the available variants and their engineering applications.

10 Minutes read

Selecting and replacing the correct timing pulleys, synchronous pulleys, and tensioning rollers

Belt systems are used where mechanical energy must be efficiently transferred. Depending on the specific requirements for power transmission, precision or even noise minimization, different belt profiles and components such as timing pulleys, synchronous pulleys or tensioning rollers are used. This article shows what to look for when making a selection.

10 Minutes read

Reamer bolts and their advantages for an aligned assembly

In many industries, from mechanical engineering to tool making and precision mechanics, the precisely tolerated positioning of components determines the quality and longevity of a product. Conventional threaded joints are often insufficient to precisely align and securely join components. This is where reamer bolts come into play – they ensure a play-free guide in bores and ensure repeatable assembly with the highest precision. In this article, you will learn why reamer bolts are the better choice for aligned joints, and the role of tolerances, thread runouts, and undercuts for optimal assembly.

7 Minutes read

LX Units - Calculating service life using preselection and calculation tool

Industrial reliability and longevity are key – especially for linear units that operate under high loads and in demanding production environments. But how can you accurately determine the service life of a linear unit? This blog post will show you how to precisely calculate the service life and what factors affect the durability of your systems. Avoid unplanned downtime, optimize your maintenance intervals, and rely on the precise design of your linear components.

19 Minutes read

Cylinder pins / tension pins / offset pins - presentation of DIN and ISO standards according to form

Cylinder pins and tension pins are connecting elements for mechanical components. Standards and norms, such as DIN EN ISO 2338 or ISO 8734 for cylindrical pins or DIN EN ISO 8752 for spring pins, define geometry, tolerances, and application areas. Particularly in mechanical engineering, pinning is a reliable method for connecting components permanently and free of play without having to use screw connections. In this article, we look at different forms of connecting pins and their standardization. We also discuss chamfers and surface finishes. In addition, we present differences in standardization and what you need to consider if you want to use pins with different standards.

9 Minutes read

Shaft Couplings and Joints - Compensation of Angular and Radial Offset

In drive technology, flexible shaft couplings and shaft joints are essential to transmit torque between two shafts – especially when the shafts are not exactly aligned or when vibrations and sudden load changes occur in the system. This article explains the difference between shaft joints and flexible shaft couplings, what each component can be used for, and what variants there are.

9 Minutes read

Connectors - Types and applications in industry

Connectors are the invisible backbone of modern industrial equipment – they ensure reliable transmission of power, signals and data. Whether it’s high-performance power connectors, precise signal connections, or highly shielded data connectors, every industrial application has specific material, design, and protection requirements. In this article, we will highlight the different types of connectors, their uses, and what to look for when selecting the right connector.

10 Minutes read

Plugs and connectors for sensor cables

Plugs, connectors, and sensor cables affect the reliability and efficiency of systems in modern industrial automation. But what types of sensors are available and how do you choose the right sensor cable? How is the connection of sensor connectors optimally implemented to ensure secure data transmission? In this blog post, we’ll explore the different connector types, highlight commonly used connectors, and explain some variations of coding M12 sensor connectors – everything you need to know to choose the right connection for your applications.

8 Minutes read

Specialty cables in mechanical engineering - Types of connection, control cables and their applications

In industry, cables and lines ensure safe and efficient signal and energy transmission. But which cable is suitable for which application? Whether it’s a power cable, data cable or hybrid solution, the right choice depends on factors such as flexibility, insulation material, shielding and compliance with (inter)national standards. In this article, we will introduce you to different types of wires and cables in an overview, explain their structure and give you a decision-making aid for selecting wires.

9 Minutes read

Profile Rail Guides - Installation and Maintenance of Linear Guides

How do you achieve the optimum ratio of precision to efficiency when installing and maintaining profile rail guides? In our blog, we highlight different installation methods, explain the difference between mounting and reference surfaces, and provide valuable tips for precise alignment. You will also learn about permissible mounting deviations and how regular maintenance or even maintenance-free concepts can affect the service life of your linear guides.

9 Minutes read

Profile Rail Guides - Allowable Loads of Linear Guides

In the industrial environment, precision and reliability count – especially for profile rail guides used in demanding conditions. But how are permissible loads calculated correctly to minimize the risk of failure while maximizing efficiency? In our blog, we explain the key calculation variables such as dynamic and static load capacity and provide insights into the distribution of forces and moments. Benefit from in-depth expertise that helps you design your applications.

16 Minutes read

Safety screws - Tamper-proof screws

Screw connections can be detached independently or detached without authorization by third parties. In order to prevent this, so-called Safety screws have been developed that make it difficult or impossible to manipulate screws. In addition to safety screws with special screw heads, there are also other design options. In this article you will find everything necessary to protect your screw connection from theft or tampering in the future.

8 Minutes read

Profile Rail Guides - Calculation of the Service Life of a Linear Guide

In industrial automation and mechanical engineering, profile rail guides are the backbone of precise and efficient motion. But how long do they really last – and what factors affect their lifespan? Read our blog to learn which types of service life are relevant, the advantages and disadvantages of profile rail guides, and how to maximize the service life of your equipment through precise calculations and targeted optimizations. Read on to learn how to make careful decisions to avoid operational downtime and ensure long-term productivity.

11 Minutes read
Lightweight pneumatic coupling for PU hoses
Lightweight pneumatic coupling for PU hoses

Pneumatic Couplings and Pneumatic Pipe Fittings

Pneumatic couplings are used in pneumatic systems to connect and disconnect hoses and pipes. What types of pneumatic couplings or Which quick connectors are available, whether they are compatible with each other, and which hoses can be connected to them, you can find out in this article. In addition, the assembly and aspects of occupational safety are discussed, since there is sometimes very high pressure in pneumatic systems.

12 Minutes read

Proximity switch vs. limit switch - Differences and areas of application

In industrial automation and control technology, precise and reliable switching operations are essential. But which technology is right for your application? Mechanical limit switches offer robustness and ease of use, while non-contact proximity switches offer high precision and durability. This blog provides you with a detailed comparison of both systems, explains their operation, differences, and areas of application, and provides valuable insights into key parameters such as sensing range, switching hysteresis, and detection distance.

16 Minutes read

Linear Systems - Stability and precision by combining linear units with linear guides

In modern production and automation systems, precision and stability are critical to quality and efficiency. The right combination of linear units and linear guides not only optimizes motion accuracy, but also increases system rigidity, durability, and load capacity. In this blog, we’ll explore how you can improve the performance of your machines through the targeted selection and integration of linear units and additional guides – from optimal sizing to load sharing concepts to practical implementation strategies for demanding industrial applications.

11 Minutes read

Optimal use of linear ball bearings and linear bearings in guide systems with the highest precision

Linear guide systems are characterized by low-friction motion and the ability to absorb lateral forces without being severely deformed. Linear ball bearings and linear bearings are used in guiding systems where precision, long life, and maintenance-free operation are essential.

6 Minutes read

Power connectors - Types and applications in Industry

In industrial production, reliable and high-performance connectors are essential to safely power machines, motors, and control systems. Power connectors play a special role in this process, from CEE connectors that provide a standard-compliant power supply to hybrid connectors that combine power and data transfer in a single interface. In this blog, you’ll learn what matters when selecting, isolating, and shielding power connectors, and how they help improve efficiency and reliability in industrial applications.

8 Minutes read
Example of a feeler gauge
Example of a feeler gauge

Gauge design explained: Inspection fixtures for quality assurance

Gauges in mechanical engineering and modern manufacturing play a central role in meeting the highest quality requirements and standards. Test gauges guarantee fast and accurate test processes without having to rely on complicated measuring technology. Inspection fixtures for material testing machines are easily adaptable to individual components. But what types of gauges and test fixtures are there? How are these structured and what components and materials are suitable when creating such a test fixture? Learn all about this in this article.

9 Minutes read

Couplings and Shaft Couplings - Selection Procedure by Motor, Torque, Torsion and Assembly Procedure

Shaft couplings are central components in drive technology and mechanical engineering because they connect shafts and enable efficient power transmission. The selection of the appropriate shaft coupling, such as e.g., a linear coupling as a non-rotary coupling, can, however, be difficult due to the wide variety of coupling types. This article introduces various selection criteria, such as motor power, required torque, and torsional characteristics, and provides guidance on designing the perfect shaft for your application.

12 Minutes read