Ball screw drives - accuracy by preloading

Ball screw drives convert rotary motion into precise linear motion or vice-versa. They are often used as a drive element. Positioning accuracy is critical when using ball screw drives. One way to increase the positioning accuracy of a ball screw drive is to reduce the play between the spindle and nut with a preload. However, since this preload also changes the ease of movement of the system, there are ball screw drives with adjustable preload. The system can be preloaded to such an extent that the permissible axial play between the ball nut and the threaded spindle is achieved without overly limiting the free movement. Preloading can achieve positional accuracy within a few micrometers. In this article, you will learn how this works and what accuracy classes there are.

8 Minutes read

Linear motion components - Things worth knowing about guides, screw drives and more

These include linear motors, linear actuators, linear axes, and other components that allow linear motion. Linear motors are specially designed motors that generate linear motion. They generate forces to move loads along a linear track.

10 Minutes read

Tutorial: Modulus of elasticity of steel – Materials science

Steel is an important material in modern industry and is used for a variety of applications. A crucial property to consider when using steels is their elasticity. The modulus of elasticity or Young’s modulus indicates how much stress is needed to achieve a certain degree of elongation. In this article we will look at the different types of steels and their respective elastic moduli.

5 Minutes read

Properties of plastics – Which plastics are suited for mechanical engineering?

Technical plastics are an indispensable part of modern industry. In custom machine construction in particular, they find a wide range of applications because they have a high degree of flexibility and formability. It is important to know what properties plastics must have in components and standard parts in custom machine construction. This article describes the most important applications for plastics in mechanical engineering.

4 Minutes read

Tolerance classes iaw. ISO 22081 and DIN ISO 2768: Optimized use of general tolerances

Tolerances are an essential aspect for manufacturing mechanically moving parts, as they ensure the correct interaction of components. General tolerances and their tolerance classes are used to simplify drawings. The standard DIN ISO 2768 specifies tolerances. Many design engineers use general tolerances as a simplified variation of tolerances to facilitate the design process.

10 Minutes read

Form and position tolerances iaw. ISO 1101 and Japanese standard JIS B 0001: The most important information

Form and position tolerances are technical specifications that ensure uniform handling of dimensions and tolerances in manufacturing. They are mainly used in the manufacture of components in order to ensure the accuracy of parts.

6 Minutes read

Low-reflective surfaces – LTBC and other options

Reflective surfaces can cause malfunctions in certain applications and even influence the results, e.g. in quality control or dimensional inspections. This should be taken into account when selecting a surface. But how can reflections be minimized? This article presents various options for surface treatment and surface coating. Low Temperature Black Chrome Plating, LTBC or also black chrome process, is explained in particular.

10 Minutes read

Machining processes and associated surface roughness

The correct surface finish significantly influences the functionality, service life and manufacturing costs of components. In this blog, you will learn everything you need to know – from the basics of surface roughness to measurement methods and international standards to hands-on examples of how roughness is called out in drawings and what machining methods deliver the desired quality. Immerse yourself in the world of precision and find out why even micrometers can make all the difference!

8 Minutes read

Erosion and corrosion in mechanical engineering

Corrosion and erosion affect the service life and performance of components. But what is actually the difference between erosion and corrosion? What types are there? And how can these forces be counteracted? The following article examines this in more detail.

8 Minutes read

The most important plastic injection molding parameters – Optimization for maximum efficiency

The plastic injection molding process is a core of modern manufacturing technology and permits an immense range of high-quality components for a wide variety of industries. But the path from granulate to the finished component presents numerous challenges. What critical components and parameters play a role? What are the most common problems that can occur and how can they be efficiently remedied? Find answers to these questions in this blog.

8 Minutes read

Precise measurements of fitting threads

Precise measurements of fitting threads are crucial for avoiding expensive leaks and system failures. In our blog, you will learn what measuring tools are truly important and which frequent errors you should absolutely avoid when measuring threads. Read more and get valuable tips for error-free joints in your industrial applications.

7 Minutes read

Properties of and working with dial gauges

Dial gauges are essential tools in industrial manufacturing and quality control. But how do you get the most out of them? In this blog, you will learn everything you need to know in order to make the best use of your dial gauges: from the most important features, to reading and clamping correctly, to avoiding measurement errors. You will also receive valuable tips on maintenance, care and calibration, so that your dial gauges work accurately for the long-term.

8 Minutes read

7 steps for selecting a swivel castor

Swivel castors give mobility to objects of all kinds. Mechanical engineering and plant construction, in particular, often require objects to be transported over long distances. Thanks to swivel castors, this is easy and efficient. This article introduces important selection criteria for swivel castors.

10 Minutes read

Details of elastomer inserts for couplings

Elastomer couplings are a type of shaft coupling. They transfer torque between two shafts and perform tasks such as power transmission, compensating alignment errors, but also damping of shocks and vibrations. Elastomer couplings ensure optimal power transmission by using various materials, and also based on their material properties and shape. The properties of the respective elastomer coupling simultaneously prevent vibrations of the drive shaft from being transmitted to the coupled shaft. The following article discusses which properties these are, how the hardness of elastomers is determined and what application examples there are.

7 Minutes read

Sealing ball bearings – Seals, sealing washers and cover washers

Ball bearings are critical components in many machines and equipment and play a central role for low-friction movement of parts. Design-based protection of rolling bearings against overload and failure due to overheating, contamination and external influences is therefore one of the fundamental tasks of a design engineer. Ball bearings can for example be sealed or one can use roller bearings already sealed by the factory to achieve the longest possible service life. To minimize friction and wear, it is necessary to ensure that bearings are sufficiently lubricated. As part of maintenance, the ball bearings must therefore be checked and relubricated as needed. However, modern industrial technology increasingly uses self-lubricating or non-serviceable sealed rolling bearings, which are already equipped by the manufacturer with corresponding sealing elements and lubricant deposits.

8 Minutes read

Rollers and wheels for industrial uses – Construction and applications

In mechanical engineering and in general automation processes, it is essential that materials and construction components are transported quickly and efficiently from A to B. This requires purposeful guidance and alignment along the conveying paths. Rollers and also drums contribute significantly toward fulfilling these functions. This article examines which types of materials are used and for which specific applications rollers are used.

12 Minutes read

Industrial material handling equipment

Material handling equipment ensures that materials and products move efficiently, safely and reliably from one point to the next. From manufacturing to stockholding and the packaging industry, material handling systems are critical for optimizing processes and improving productivity. The following blog highlights different types of material handling equipment and its specific benefits for specific applications. We also answer the question of which points play a role for selecting the correct material handling system.

7 Minutes read

Wheel conveyors, roller conveyors and roller strips – Construction, function and advantages

Material handling engineers rely on roller conveyors to efficiently transport products, goods and materials. They are invaluable, particularly in logistics, but also in many other industries and various manufacturing processes. This article discusses how roller conveyors are constructed, how they work and which variants there are.

9 Minutes read

Technical ceramics in practice – Ceramic screws, ceramic bearings and hybrid bearings

Technical ceramics are ceramics used in specialized technical applications. Due to their special properties, such as resistance to high temperatures and chemicals, they are often the better choice in certain applications than components made of metal, for example. This article shows some of the possible applications and discusses the material composition and production of technical ceramics.

8 Minutes read

Industrial gas compression springs – Design, advantages and uses

Gas compression springs support moving parts or compensate weight. They are used, for example, for doors, hatches or swivel arms. Especially in mechanical engineering and plant engineering, it can be useful for safety reasons to provide certain components and machines with hatches. Gas springs support opening and closing these, especially on heavy hatches and doors. This blog article explains how they work, what variants there are and where else they can be used.

10 Minutes read