Representing threads in technical drawings

The correct representation of threads in technical drawings serves as a basis for technical communication between participating trades. Extensive information can be presented in a clear and internationally understandable manner and thus supports the smooth process in mechanical manufacturing, production and assembly. In this article, you will learn how threads and bore holes are shown in detail in mechanical engineering.

8 Minutes read

Calculating shear strengths and tensile strengths for screws

Shear strength and tensile strength are two important parameters for selecting and using screws. Screws are used to connect components in a friction-locking manner and to withstand mechanical loads. In order to ensure that screws meet the required strength requirements in a given application, it is important to know what shear strength and tensile strength are and how they are calculated.

8 Minutes read

Understanding bearing damage – Causes, failure mode and prevention

Rolling bearings are robust and reliable components in mechanical engineering and custom machine construction. Under certain conditions, however, bearing damage to these widely used machine elements can occur, usually resulting from unusual behavior during operation. In the worst case, bearing damage can result in a complete failure of the rolling bearings, which can result in unwanted downtime. Therefore, it is important to detect the first signs of rolling bearing damage early on and to remedy their causes. In this article, we discuss the symptoms of bearing damage, its causes and typical failure modes.

10 Minutes read

Parallel keys and tapered keys – Standards and norms (OLD+URL Redirect)

Parallel keys and tapered keys are two common connecting elements in the mechanical engineering industry. They are used to create a force-locking connection between two components. In this article, the two key types are examined in more detail and their areas of application are explained.

1 Minutes read

Metals and surface treatments – an overview (OLD+URL Redirect)

Industrial surface treatment is a process where a surface of a workpiece is treated to improve or change its mechanical, chemical or visual properties.

1 Minutes read

How to select the right component surface – expert knowledge of surface roughness and surface hardness (OLD+URL Redirect)

Surface roughness and surface hardness are important properties that must be taken into account when selecting components. Although there are different methods for measuring the roughness or coarseness of a component surface, these measurements often have to be converted to a standard measure.

1 Minutes read

Steel materials, steel and industrial materials: A guide to choosing the best steel for your applications

Industrial materials are very diverse and include metal (e.g. steel), polymers, glass and composites. It is important to take a look at these materials as they are used for a wide range of applications.

5 Minutes read

Shaft couplings – Basics and areas of application (OLD+URL Redirect)

This blog article provides an introduction on how couplings work and the different types in use today.

1 Minutes read

Optimal use of linear ball bearings and linear bearings in linear guide systems with maximum precision

Linear guide systems are characterised in particular by a low friction running behaviour and the ability to absorb transverse forces without being heavily deformed. Linear ball bearings and linear bearings are used in guide systems where maximum precision, long service life and maintenance-free operation are important.

6 Minutes read

Shaft types in mechanical engineering – Linear shafts, rotary shafts, rods and how to make the right choice

Shafts are an important part in the engineering industry as they connect different components. Different types of shaft are used in mechanical engineering, including linear shafts, rotary shafts, and rods. There are several factors to consider when selecting the best shaft for a specific application. These include the type of application, the performance requirements and the type of shaft that is best suited for the application. If you make the right choice, you can be sure that the machine will work efficiently and achieve the desired results.

6 Minutes read

Select the optimal bearings for rotary shafts and torsion shafts

Bearings are an essential component for fixing and guiding rotary and torsion shafts. They can have a major impact on the service life of your system and machines, which is why it is important to make the right choice. This article describes which bearings are best suited for rotary and torsion shafts and what you need to consider when selecting them.

6 Minutes read

Understanding rotary shafts, axes and motor shafts: A guide (OLD+URL Redirect)

Rotary shafts are an key element of modern mechanical engineering. Rotary shafts transmit rotational motions. They can be made of different materials, which are specifically selected depending on the application. Materials include stainless steel, rust-free steel and steel.

1 Minutes read

Chains and sprockets: how they work together

Chains and sprockets are important elements in the design and mechanics of machines and systems. They are indispensable for mechanical transmission of movement and force.

10 Minutes read

Components for linear motion – key facts about drives, shafts, couplings, drives, guides and much more (OLD+URL Redirect)

Linear motors, linear actuators, linear axes, and other components enable linear motion. Linear motors are specially designed motors that generate linear motion. They generate forces to move loads in a straight line.

1 Minutes read