Screws – Overview of standard
There are different designation systems for the properties of screws. The underlying standards form the basis for classifying and designating screw types. This article briefly presents some of the different screw standards and their differences, and provides a general overview of screws in the European region.
Overview of screw standards
Standards are used for standardization and represent an agreement within a specific group that has agreed on this standard. Since many national standards have emerged over time and under the influence of historical and regional developments, they are often only commonly used and recognized in these regions. Worldwide, there are a variety of standards to ensure that screws meet specific requirements. The use of, and compliance with, standards is generally not binding, but can be contractually agreed or mandated by lawmakers. These standards are essential to ensure the quality, safety and functionality of fasteners.
Standards
The Deutsche Institut für Normung e.V., abbreviated as DIN, is responsible for determining and updating the national DIN standards. Standardization in the European single market are aimed at European standards, abbreviated as EN. EN standards will be adopted into national standards as quickly as possible and without changes after the resolution of the European Council; in Germany they are called DIN EN. The corresponding DIN is withdrawn and replaced by the DIN EN. ISO standards are intended to facilitate worldwide standardization. Global ISO standards should categorically be adopted into EN standards without changes. As a global manufacturer with headquarters in Japan, MISUMI also produces and sells products that are standardized iaw. the national standard JIS (Japanese Industrial Standard). The respective standard describes the details of standardized screws, including diameter, (thread) length and head shape.
The following explains the screw designation iaw. DIN:
- DIN 933 M 10 x 80 A2-70
The abbreviation DIN 933 stands for hex screws with thread up to the head. M10 x 80 refers to a 10 mm (M10) diameter metric screw with a 80 mm length. A2-70 describes a stainless steel specification that not only indicates the quality and corrosion resistance of the material, but also a minimum tensile strength of 700 N/mm². In addition to this information, the respective standards generally contain the relevant thread tables.
DIN screws
DIN standards are best known in Germany. In the past, many screws have already been standardized in Germany using a DIN standard. For example, DIN 933 applied to hex screws. The aim of establishing global standards has led to the development of international standards (ISO standards) for a growing number of applications and to the replacement of DIN standards with corresponding EN standards or ISO standards. Nevertheless, DIN standards apply whenever there is no corresponding successor standard as DIN EN or ISO standard (DIN EN ISO).
ISO screws
ISO regulates various screw standards at an international level. Many ISO standards largely contain the same regulations as the previously valid DIN standards. However, they are used in several countries. The successor standards for DIN 931 and DIN 933 are, for example, DIN EN ISO 4014 and DIN EN ISO 4017. Other standards are:
- ISO 4762 for socket head cap screws with hex socket
- ISO 7380 for flat head screws with hex socket
- ISO 2009 for countersunk screws with slot
- ISO 7045 for pan head screws with Phillips cross slot
- ISO 965 for general-purpose threads
In mechanical engineering, hexagon head screws in accordance with DIN EN ISO 4014 and cylinder screws in accordance with DIN EN ISO 4762 are most commonly used.
Screws iaw. JIS
The Japanese Industrial Standard (JIS) standard is published by the Japanese Standards Association. Many screws are also standardized in the metric unit system. In addition to various overlaps of screws that are standardized iaw. the Japanese JIS standard with those that were manufactured iaw. DIN or ISO, there are sometimes significant differences in certain screw types. In some cases, special tools are required for the JIS standard.
Common JIS standards for threads include:
- JIS B 0205-1:2001 for general metric thread (standard angle shape)
- JIS B 0205-2:2001 and JIS B 0205-3:2001 for general-purpose metric threads
- JIS B 0205-4:2001 for general metric thread (standard dimensions)
- JIS B 0207:1982 for metric fine threads
MISUMI offers screws of all standards.
Meaning of the differences
Differences in standardization primarily affect the choice of tools. As a rule, JIS screws are compatible with tools that are adapted to DIN screws. Nevertheless, the so-called cam-out effect (tool slipping out of the screw head) can occur, for example, on Phillips screws iaw. the JIS standard when using unsuitable tools. It is therefore recommended to use special JIS tools for JIS screws. This maintains ease of movement and screws are not unnecessarily damaged.
Thread types and their differences
A thread is a helical elevation or recess on a screw, a bolt or another fastening element. The threads are also subject to the standards. The following parameters describe the threads in more detail:
- Thread tips: are the outer edges of a thread.
- Outer diameter: also called nominal diameter, is the diameter of the outer threaded part. Thread-outer diameter tables are used to determine the required outer dimension.
- Core diameter: also called core hole diameter. When cutting threads, a core hole bore ensures correct centering. The core hole determines the smallest inner diameter of the subsequent thread. There are various threaded core hole tables for reading the associated nominal dimensions and pitches.
- Edges: ae the oblique or inclined sides of a thread that form the helical elevations or recesses and extend along the thread profile.
- Pitch: the thread pitch is a dimension that indicates the distance between successive threads or elevations of a thread. It is defined differently depending on the thread. For metric threads, the thread pitch results, for example, from the path traveled in one revolution. For inch threads, for example, the thread pitch is determined by the number of threads per inch.
- Pitch angle: the pitch angle is the angle at which the thread flanks of a thread rise or fall (as seen along the thread profile).
- Start: is the continuous recess in the helix (around or in a bolt/nut).
Thread shapes are different worldwide and often lead to challenges in the compatibility of screws and their applications. Germany and many other European countries primarily use metric threads, which are characterized by a standardized pitch and angle. This standardization facilitates identification and application. In contrast, the USA traditionally uses inch threads. In the USA, Unified Thread Standard (UTS) threads are particularly common, which differ significantly in their classification and dimensions from the metric systems. In Japan, the metric system for threaded connections is widely used. For pipe threads, inch threads are typically used internationally for all standardization regions. The different thread pitches, angles and dimension systems (metric vs. inch) have the effect that the usability of screws from different regions is often limited or not possible at all. Due to the historical development of thread standards worldwide, it is essential to precisely check the thread before using screws. This prevents damage and ensures the functionality of connections.
Different screw head types
In addition to the actual thread, the heads of the screws also play an important role. Various screw heads and their advantages are presented below:
Round head
Round head screws have a round head that extends beyond the surface of the material into which they are screwed. The head can be either completely round or slightly hemispherical, depending on the design. The round shape reduces the risk of injury, offers a larger contact surface and allows for uniform load distribution.
Cylinder head
The cylinder head is a flat screw head with a cylindrical surface. It is threaded in from above, which is why it is suited for use in difficult-to-reach areas. DIN standards 4762 and 912 or JIS B 1176 apply for hexagon socket head cap screws. Flat head screws are a special shape of cylinder head screws.
Hexagon head
The hexagon head has six sides and a flat surface with six corners. It is easy to grasp and tighten with a hex wrench or an open-face wrench. Hexagon head screws are suitable for high torque applications. Unlike round head screws driven from the inside, a hexagon head screw is tightened with the force that acts on the head from the outside. DIN standards 4014 and 933 or JIS B 1180 apply to hexagon head screws.
Countersunk head
Countersunk screws have a tapered screw head that allows the screw to be countersunk into the material. They are often used when the screw head needs to be flush with the surface of the material to provide a smooth surface without protruding parts. Countersunk screws reduce the risk of tripping and injury. DIN ISO 10642, for example, applies for countersunk screws.
Pan head
Pan head screws have a semicircular head. This head distributes the load evenly over the total surface area and stresses the material less. Penetration of the screw head into the workpiece is avoided, the service life is extended. DIN ISO 7380-2, for example, applies for pan head screws.
Knurled screw
Knurled screws are characterized by a head with a knurled surface that provides increased grip. This special texture makes it possible to tighten or loosen the screw by hand without tools. Knurled screws are particularly suitable for applications that require frequent manual adjustment or for areas where quick access without tools is important, such as on housings for electronic equipment or adjustment mechanisms.
Wing head
Wing screws have two lateral, wing-like protrusions that allow easy tightening and loosening by hand without tools. This screw head is particularly useful for applications that require quick and frequent adjustment, e.g. when attaching to machine covers or when adjusting various equipment. The wide wings offer good handling with corresponding leverage effect, which facilitates tightening and loosening, even if greater forces are required.
Eye bolts
Eye bolts, also called ring bolts, are characterized by a circular ring that looks like an "eye" on the head. This design allows hooks to be engaged or cables to be threaded through, thus supporting a variety of mounting and lifting tasks. They are particularly useful for applications that require suspension, such as transporting heavy loads. Eye bolts provide a secure attachment point and are designed to function reliably even under heavy loads. Thanks to their robust construction, they can withstand tensile and also shear forces.
Other head shapes
In addition to the classic head shapes, such as round, cylinder and hexagon head screws, there are also less common, but nevertheless important, head shapes such as square and triangular screw heads. Square head bolts offer high resistance to twisting and are particularly popular in the assembly industry, which requires robust connections. Triangular screws, which require special tools for tightening, offer additional security against unauthorized unthreading and are therefore often used in safety devices. Technological advances and increasingly specific requirements of various industries have led to the development of additional screw head shapes that can offer optimized solutions for special assembly or safety requirements.
Various screw drives
Choosing the right screw drive is crucial for efficient and safe assembly operations. The most common types are slotted screws, Phillips screws, socket head cap screws, and external hex screws. Slotted screws are one of the oldest screw shapes and are often used for simple applications that do not require high torque. Phillips screws provide better support and are often used in electrical engineering and in general mechanical engineering. Hex cap screws, also known as Allen screws, provide even greater torque transfer and are often used for connections requiring high strength. External hex screws, on the other hand, are ideal for applications that use wrenches and require higher torque. Each screw connection requires specially shaped tools that are precisely matched to the fit and shape of the screw connection in order to ensure optimal support and optimal torque transfer. For example, hexagon socket and Torx drives require wrenches or bits that fit into the screw profile and prevent head damage. These tools are available in metric and inch systems, making them easy to use in various regions and industries. When using JIS screw drives, it is recommended to order a special JIS screwdriving tool.
Overview of screw standards
Without claiming to be complete, the following table shows the various screw standards:
| Screw designation (data as of 04/2024) | DIN | DIN EN | DIN EN ISO | ISO |
|---|---|---|---|---|
| Socket Head Screws with slot | DIN 84 (withdrawn) | 1207 | ||
| Slotted flathead screws | DIN 85 (withdrawn) | 1580 | ||
| Lens countersink wood screws with slot | DIN 95 | |||
| Half-round wood screws with slot | DIN 96 | |||
| Countersink wood screws with slot | DIN 97 | |||
| T-screws with square head (hammerhead screw) | DIN 186 | |||
| T-screws with tab (hammerhead screw) | DIN 188 | |||
| T-screws | DIN 261 | |||
| Wing bolts (US and German standard) | DIN 316 | |||
| Capstan screws | DIN 404 | |||
| Grub screws with slot and boss | DIN 417 (withdrawn) | DIN EN 27435 | ISO 7435 | |
| Grub screws with slot and shank | DIN 427 (withdrawn) | DIN EN ISO 2342 | ISO 2342 | |
| Eyelet screws | DIN 444 | |||
| Knurled screws, high shape | DIN 464 | |||
| High knurled screws with slot (replaced by DIN 464) | 465 (withdrawn) | |||
| Square bolts with collar | DIN 478 | |||
| Square bolts with short boss | DIN 479 | |||
| Square bolts with collar and oval half dog point | DIN 480 | |||
| Stone screws | DIN 529 | |||
| Grub screws with slot and truncated cones | DIN 551 (withdrawn) | DIN EN ISO 4766 | ISO 4766 | |
| Grub screws with slot and point | DIN 553 (withdrawn) | DIN EN 27434 | ISO 7434 | |
| Hex screws with tappet and small hexagon | DIN 561 | |||
| Hex screws with pointed neck and small hexagon | DIN 564 | |||
| Hex wood screws (lag bolts) | DIN 571 | |||
| Steel and stainless steel lifting eyebolts | DIN 580 | |||
| Lifting eyebolts, forged steel, grade 4 | DIN EN ISO 3266 | ISO 3266 | ||
| Hexagon head screws with shank - product class C | DIN 601 (withdrawn) | DIN EN ISO 4016 | ISO 4016 | |
| Flat round screws with square neck (neck bolts) | DIN 603 (M5 to M20) | ISO 8677 | ||
| Countersunk screws with nose | DIN 604 (M6 to M24) | |||
| Hex reamer bolt with long threaded pin | DIN 609 | |||
| Knurled screws, low-profile shape | DIN 653 (M1 to M10) | |||
| Stud bolts - thread-in end ≈ 2 d | DIN 835 | |||
| Screw plugs with internal drive - Tapered Thread | DIN 906 | |||
| Screw plugs with collar and internal drive - cylindrical thread | DIN 908 | |||
| Screw plugs with external hex - conical thread | DIN 909 | |||
| Screw plugs with collar and external hex - cylindrical thread | DIN 910 | |||
| Socket cap screws with hex socket, metric thread | DIN 912 (withdrawn) | DIN EN ISO 4762 | ISO 4762 | |
| Grub screws with hexagon socket and conical dome | DIN 913 (withdrawn) | DIN EN ISO 4026 | ISO 4026 | |
| Grub screws with hex socket and flattened point | DIN 914 (withdrawn) | DIN EN ISO 4027 | ISO 4027 | |
| Grub screws with hex socket and boss | DIN 915 (withdrawn) | DIN EN ISO 4028 | ISO 4028 | |
| Grub screws with hex socket and cup point | DIN 916 (withdrawn) | DIN EN ISO 4029 | ISO 4029 | |
| Panhead screws with slot and small head | DIN 920 | |||
| Panhead screws with slot and large head | DIN 921 | |||
| Panhead screws with slot and point | DIN 923 | |||
| Hexagon head screws with shank | DIN 931 (withdrawn) | DIN EN ISO 4014 | ISO 4014 | |
| Fasteners - hexagon head screws with thread up to head - product classes A and B | DIN 933 (withdrawn) | DIN EN ISO 4017 | ISO 4017 | |
| Stud bolts - threaded-in end ≈ 1 d | DIN 938 | |||
| Stud bolts - threaded-in end ≈ 1.25 d | DIN 939 | |||
| Hexagon head screws with shank and metric fine thread | DIN 960 (withdrawn) | DIN EN ISO 8765 | ISO 8765 | |
| Hexagon head screws with thread up to head; fine thread | DIN 961 (withdrawn) | DIN EN ISO 8676 | ISO 8676 | |
| Countersunk screws with slot | DIN 963 (withdrawn) | DIN EN ISO 2009 | ISO 2009 | |
| Raised countersunk screw with slot | DIN 964 (withdrawn) | DIN EN ISO 2010 | ISO 2010 | |
| Countersunk screws (unit head) with shape H or shape Z cross slot | DIN 965 (withdrawn) | DIN EN ISO 7046 | ISO 7046 | |
| Raised countersunk screws (unit head) with shape H or shape Z cross slot | DIN 966 (withdrawn) | DIN EN ISO 7047 | ISO 7047 | |
| Raised countersunk screws with collar and cross slot | DIN 967 | |||
| Combination screws made of steel with flat washers | DIN 6900 (withdrawn) | DIN EN ISO 10644 | ISO 10644 | |
| Combination tapping screws with flat disc | DIN 6901 (withdrawn) | DIN EN ISO 10510 | ISO 10510 | |
| Socket cap screws with hex socket and reduced max. load - low-profile head, with key guide | DIN 6912 | |||
| Hex screws with flange, heavy series | DIN 6921 (withdrawn) | DIN EN 1665 | ||
| Screws with control thread and thin shank (as captive feature) | DIN 6929 | |||
| Self-tapping screws for metric ISO thread - Part 1: | DIN 7500 | |||
| Self-tapping screws for metric ISO thread - part 2 | DIN 7500-2 | |||
| Lens countersink self-drill screws with cross slot with self-tapping thread | DIN 7504 (withdrawn) | DIN EN ISO 15483 | ISO 15483 | |
| Self-tapping screws - hex screws, slotted screws | DIN 7513 | |||
| Self-tapping screws - cross head screws | DIN 7516 | |||
| Screw plugs with external hex – lightweight type – cylindrical thread | DIN 7604 | |||
| Screws with control thread with thin shank | DIN 7964 (withdrawn) | |||
| Hexagon reamer bolt with hex nut for steel structures | DIN 7968 | |||
| Cylinder self-tapping screws with slot | DIN 7971 (withdrawn) | DIN EN ISO 1481 | ISO 1481 | |
| Countersunk self-tapping screws with slot | DIN 7972 (withdrawn) | DIN EN ISO 1482 | ISO 1482 | |
| Lens countersink self-tapping screws with slot | DIN 7973 (withdrawn) | DIN EN ISO 1483 | ISO 1483 | |
| Hexagonal self-tapping screws | DIN 7976 (withdrawn) | DIN EN ISO 1479 | ISO 1479 | |
| Raised self-tapping screws with cross slot | DIN 7981 (withdrawn) | DIN EN ISO 7049 | ISO 7049 | |
| Countersunk self-tapping screws with cross slot | DIN 7982 (withdrawn) | DIN EN ISO 7050 | ISO 7050 | |
| Lens countersink self-tapping screws with cross slot | DIN 7983 (withdrawn) | DIN EN ISO 7051 | ISO 7051 | |
| Socket cap screw with hex socket with low-profile head with reduced max. load | DIN 7984 | |||
| Flathead screws with shape H or shape Z cross slot | DIN 7985 (withdrawn) | DIN EN ISO 7045 | ISO 7045 | |
| Screws with flattened semicircular head with hexagon socket | DIN EN ISO 7380-1 | ISO 7380-1 | ||
| Screws with flattened semicircular head with hexagon socket and collar | DIN EN ISO 7380-2 | ISO 7380-2 | ||
| Screws with flattened semicircular head with hexagon recess | DIN 34805-1 | |||
| Screws with flattened semicircular head, with collar and hexagon recess | DIN 34805-2 | |||
| Countersunk screws with hexagon socket | DIN 7991 (withdrawn) | DIN EN ISO 10642 | ISO 10642 | |
| Lens countersink wood screws with cross slot | DIN 7995 | |||
| Half round wood screws with cross slot | DIN 7996 | |||
| Countersunk wood screws with cross slot | DIN 7997 | ISO 7093 | ||
| Plate screws and plate washers for fastening components to belts | DIN 15237 |