Product Info

Cylinder pins / tension pins / offset pins - presentation of DIN and ISO standards according to form

Cylinder pins and tension pins are connecting elements for mechanical components. Standards and norms, such as DIN EN ISO 2338 or ISO 8734 for cylindrical pins or DIN EN ISO 8752 for spring pins, define geometry, tolerances, and application areas. Particularly in mechanical engineering, pinning is a reliable method for connecting components permanently and free of play without having to use screw connections. In this article, we look at different forms of connecting pins and their standardization. We also discuss chamfers and surface finishes. In addition, we present differences in standardization and what you need to consider if you want to use pins with different standards.

9 Minutes read

Shaft Couplings and Joints - Compensation of Angular and Radial Offset

In drive technology, flexible shaft couplings and shaft joints are essential to transmit torque between two shafts – especially when the shafts are not exactly aligned or when vibrations and sudden load changes occur in the system. This article explains the difference between shaft joints and flexible shaft couplings, what each component can be used for, and what variants there are.

9 Minutes read

Plugs and connectors for sensor cables

Plugs, connectors, and sensor cables affect the reliability and efficiency of systems in modern industrial automation. But what types of sensors are available and how do you choose the right sensor cable? How is the connection of sensor connectors optimally implemented to ensure secure data transmission? In this blog post, we’ll explore the different connector types, highlight commonly used connectors, and explain some variations of coding M12 sensor connectors – everything you need to know to choose the right connection for your applications.

8 Minutes read

Connectors - Types and applications in industry

Connectors are the invisible backbone of modern industrial equipment – they ensure reliable transmission of power, signals and data. Whether it’s high-performance power connectors, precise signal connections, or highly shielded data connectors, every industrial application has specific material, design, and protection requirements. In this article, we will highlight the different types of connectors, their uses, and what to look for when selecting the right connector.

10 Minutes read

Specialty cables in mechanical engineering - Types of connection, control cables and their applications

In industry, cables and lines ensure safe and efficient signal and energy transmission. But which cable is suitable for which application? Whether it’s a power cable, data cable or hybrid solution, the right choice depends on factors such as flexibility, insulation material, shielding and compliance with (inter)national standards. In this article, we will introduce you to different types of wires and cables in an overview, explain their structure and give you a decision-making aid for selecting wires.

9 Minutes read

Profile Rail Guides - Allowable Loads of Linear Guides

In the industrial environment, precision and reliability count – especially for profile rail guides used in demanding conditions. But how are permissible loads calculated correctly to minimize the risk of failure while maximizing efficiency? In our blog, we explain the key calculation variables such as dynamic and static load capacity and provide insights into the distribution of forces and moments. Benefit from in-depth expertise that helps you design your applications.

16 Minutes read