Linear Systems - Stability and precision by combining linear units with linear guides
In modern production and automation systems, precision and stability are critical to quality and efficiency. The right combination of linear units and linear guides not only optimizes motion accuracy, but also increases system rigidity, durability, and load capacity. In this blog, we’ll explore how you can improve the performance of your machines through the targeted selection and integration of linear units and additional guides – from optimal sizing to load sharing concepts to practical implementation strategies for demanding industrial applications.
Linear System, Linear Unit, Linear Guide
A linear system is a mechanical assembly that provides precise, straight-line motion. It combines various components such as linear units, linear guides, linear actuators such as ball screws, toothed belts or linear motors, and control electronics. Linear systems are used in mechanical engineering, automation, robotics, and many other industries where high precision and repeatable motion is required.
A linear unit is a pre-assembled, drive-based motion unit that realizes controlled linear motion. It typically consists of a drive system (e.g., ball screw drive or timing belt drive) and an integrated guide that stabilizes travel. Linear units are used as linear modules in machines and equipment to efficiently implement precise positioning or automated movements.
A spindle-driven linear unit offers exceptional positioning accuracy and is ideal for moderate speed applications such as CNC machines or metrology. Direct-drive linear units with linear motors, on the other hand, enable highly dynamic motion with maximum precision and are often used in high-speed motion automation systems. A linear unit with a timing belt is ideal for fast and long travels, as it ensures high dynamics with low maintenance. Heavy-duty linear units are used for particularly high loads; they are particularly robustly designed and specially designed for higher loads.
A linear guide is a mechanical component without its own drive. It enables a low-friction and exact linear movement by guiding a movable element (e.g. a carriage) along a fixed path. It usually consists of guide rails and carriages with ball or roller bearings. Linear guides provide stability, reduce friction, and enable high load capacities while maintaining accuracy. In industrial applications, they are critical to the accuracy and longevity of linear systems.
Criteria for Selecting Linear Units
In addition to obvious parameters such as stroke, load or positioning accuracy, a number of other factors play an important role in selecting a suitable linear unit. Particularly when it comes to economic and technical optimization in industrial applications, it is worth looking a little more closely here. An often underestimated aspect is the position of the load and the resulting actual direction of action of the forces generated by applied loads. They directly influence the transmission of force into the guide and drive. While centrally placed loads result in uniform loading and minimal friction, lateral or eccentric forces generate additional tilting moments that can lead to increased wear and reduced service life. In such cases, design measures such as additional guides or wider carriage mounts are a suitable way to increase stability and thus ensure a long service life of the entire linear system.
Another central criterion is the travel speed: Highly dynamic applications in automation require rapidly accelerating, smooth-running linear units with the lowest possible dead weight. At the same time, the speed also influences the selection of the drive concept as well as the design of the guide. Costs and space requirements are also not to be underestimated during project planning. Compact designs enable higher integration density and save valuable space, especially in modular machine designs. Here, for example, a skillful combination of linear guide and linear unit may be a more cost-effective alternative to a larger-sized linear unit.
Serviceability and susceptibility to errors, in turn, have a direct impact on operating costs and plant availability. Easy-access lubrication points or low-maintenance designs ensure smooth operation for long periods of time. Last but not least, targeted weight savings through lightweight materials or compact assemblies can help to improve the energy balance and dynamics of the overall system.
Support through guide systems for primary load absorption
When using a single profile rail guide, rolling moments or yaw and pitch moments occur. This puts a heavy load on the carriage and causes it to tend to twist or tilt.
The load-bearing capacity for moments in the pitch direction can usually be improved relatively easily by the use of several carriages on a guide rail. At the same time, the guide becomes more resilient and resistant to rolling and yaw moments. Double rail guides are suitable to reduce and, if possible, prevent rolling torques acting on the guide carriages.
If the standard guide of a linear unit is not sufficient, additional guidance may be useful to improve overall stability, load capacity and service life. There are several ways to integrate additional guide systems to support the main load into an existing linear system. What to look for in detail – especially in terms of permissible forces and moments – is explained in our blog on Permissible Loads of Linear Guides.
Combination of two profile rail guides
The combination of two profile rail guides provides the highest precision and stability. Using two parallel profile rail guides maximizes torsional rigidity, allowing high loads to be moved with consistent precision.
In systems with two parallel, single-guided linear guides, the influence of the roll moments is reduced, but there is a residual risk of tilting or an improperly running carriage - especially in the case of eccentric load or uneven force introduction. This can lead to higher friction resistance, uneven wear, and ultimately, reduced service life. In contrast, two-way guided systems - for example, with two guide carriages on one rail - offer significantly better stability against yaw and pitch moments. With a larger footprint and better moment load capacity, the unit runs smoother, more precisely and is often more durable. Four-way-guided systems using two profile rails with two guide carriages each provide even higher rigidity, minimize occurring moments and allow excellent smoothness and repeatability even under high dynamic loads or off-center loads.
In a configuration with a single linear ball bearing on a single linear shaft, the bearing can only absorb radial forces. Roll moments cannot be supported. Moments in the pitch or yaw direction are taken up via the longitudinal axis because they consist of a lever and a radial force.
If two linear bearings are used on the same shaft, the guide property improves with regard to pitch and yaw torque (in the direction of motion), but the rolling torque still cannot be supported. Only with the use of two parallel linear guides with one or more linear bearings each does the system become stable against roll moments.
A slightly more expensive, but usually still cost-effective alternative is the combination of a linear ball bearing guided on a linear shaft with a supplementary profile rail guide. While these hybrid solutions are somewhat more expensive than purely shaft-guided systems, they are usually less expensive than solutions that rely entirely on profile rail guides with multiple carriages and rails. The combined variant also requires slightly less space than an implementation with two profile rail guides used in parallel. The simple design combines a linear shaft with a linear ball bearing parallel to a profile rail with a guide carriage. This variant provides solid guidance. The extended design uses two linear ball bearings per linear shaft and two guide carriages per profile rail. This configuration is further improved in terms of stability, smoothness and precision, since both the force transmission and the moment support are more uniform.
For applications with particularly high requirements for precision, rigidity and load capacity, purely profile-guided systems with multiple guide carriages are often the best solution. These are among the highest-quality, but also the most expensive, variants. In the configuration with two parallel profile rail guides and one guide carriage each, there is already a very good stability against pitch, yaw and rolling torques. The variant with two profile rail guides used in parallel and two guide carriages per rail is even more powerful. With a total of four carriages, the force is distributed particularly evenly across the system, which makes the unit extremely torsionally rigid. With this arrangement, almost no more moments occur in the individual carriage, since the real moment only acts as a pure force on the carriage.
Other linear system combinations
There are also numerous combination options of profile rails, guide carriages and bearing types that can be connected to one another depending on the application. Depending on the requirements for precision, rigidity, dynamics and costs, this results in customized solutions for a wide variety of applications in mechanical engineering and automation.
Parallel arrangement of two or more linear units
Another way to optimize load pickup is to arrange two or more linear units in parallel. When a single unit hits its load limit, additional units installed in parallel can share the load, minimizing deflection effects. This configuration distributes the forces more evenly, resulting in higher rigidity and extended component life. The following example shows an assembly with an integrated double profile rail guide.
Use of additional profile rail guides with separate guide carriage
An additional profile rail guide with separate guide carriage provides a more uniform load distribution. This increases the stability of the overall system, as the additional guidance provides additional support and reduces tilting moments, especially during long strokes or lateral forces.
Combination of a profile rail guide and a linear ball bearing
For applications that require good precision but do not place the highest demands on rigidity, the combination of a profile rail guide and a linear ball bearing is a more cost-effective alternative. This configuration provides a balanced combination of stability and precision while reducing costs. The linear ball bearing provides precise guidance, while the profile rail guide increases torsional rigidity and load-bearing capacity in addition to its guiding function.
Combination of a profile rail guide and a linear slide bearing
If cost is the main criterion, the combination of a profile rail guide and a linear slide bearing is one of the most cost-effective solutions. Linear slide bearings are significantly less expensive than profile rail guides and provide simple, low-maintenance guidance. However, they are unable to provide the same precision or rigidity as profile rail guides with preloaded guide carriages or other options.
Examples of linear systems
The following are two design examples:
Benefits of an additional linear guide
Combining a linear unit with an additional linear guide offers numerous advantages, especially in demanding industrial applications where stability, precision, and durability are required.
A key advantage is that the linear unit can be sized smaller, as the additional guide distributes the forces among several components, thus enabling a more compact design. This allows material savings to be realized without compromising load capacity or service life.
At the same time, the additional linear guide provides significantly increased torsional stiffness. Especially with long strokes or asymmetric loads, the risk of deflection or unwanted vibration is greatly reduced. This not only improves the overall precision of the system, but also contributes to stability under dynamic load.
Another positive effect is that the load on the actual linear unit is reduced. The guide absorbs much of the forces and moments that occur, which relieves the drive mechanism, whether it is a ball screw, a timing belt, or a linear motor. The lower mechanical stress reduces wear and extends the service life of the entire system.
In some cases, this combination may also save space depending on the design of the components used. For example, flatter and more compact designs can be realized by integrating the additional guidance into the existing machine structure. However, this benefit is highly dependent on the specific application and the chosen design.