Pipe Fittings – Types and applications
Pipe fittings are used to securely connect pipes, tubes, and hoses. They are used in pneumatics as well as in hydraulics and other fluid-carrying systems. However, suitable fittings and adapters are also available for pipes under vacuum. As an important component of these systems, it is essential that pipe fittings reliably and securely connect the components to be connected. At the same time, they are intended to permanently prevent liquids or gases from entering or exiting. This article introduces different types of pipe fittings and their possible uses, and will help you choose the best pipe fitting for your application.
Pipe connections in general
There are several ways to join pipes. The choice of available joining methods depends greatly on the subsequent accessibility of the connection, the material to be connected, the pressure and type of the medium, as well as any special requirements for the connection or the entire system. Pipe connecting elements are often called fittings. Fittings are just one of the many ways to join pipes.
In general, a distinction is made between releasable and non-releasable connections for pipe connectors. While releasable pipe connections allow for easy assembly and non-destructive disassembly, non-releasable connections can only be released by destroying part of the material. In contrast to releasable connections, non-releasable connections can therefore also not be used in accessible areas.
Releasable connections are typically made with pipe connectors such as threaded connections or screw fittings, compression fittings, flanged connections or pipe couplings. But releasable pipe connections also include sleeve connections, cuff connections and plug-in connections. Releasable connections are often referred to as fittings and couplings. Both are a subset of connectors, but differ as follows: Fittings provide a simple and permanent connection. Couplings, on the other hand, are connections for quickly connecting or disconnecting hoses and pipes. Integrated shut-off valves can be added to automatically stop flow after the pipes are disconnected.
Non-releasable pipe connections are usually somewhat more complex to fabricate than releasable pipe connections: Pipes are welded, adhesive-bonded or soldered to each other or to the appropriate pipe connectors. This type of connection is recommended especially for lines that are under heavy loads or are no longer accessible later. There are also a wide range of fittings and connectors for these purposes. This includes, for example, press fittings and sliding sleeve connections.
What basic forms of pipe connectors are there?
Pipe connectors perform various tasks: They are, for example, designed to connect, reduce or branch pipes in a pipe system. Various pipe connectors and their typical uses are shown in more detail below.
Pipe couplings
Pipe couplings allow pipes to be connected and disconnected quickly, easily and flexibly. Pipe couplings are particularly suited if pipe segments need to be separated or replaced more frequently. They are for example used in water and compressed air systems that require adjustments and maintenance. Examples of pipe couplings are: Screw-on couplings, socket unions.
Pipe manifolds
Pipe manifolds distribute media such as water, compressed air, or hydraulic fluids to multiple outlet points. In sanitation systems, they ensure the safe and efficient water supply in buildings or production facilities. Pneumatic pipe manifolds are used to supply compressed air , for example for machines, and hydraulic pipe manifolds are used to supply hydraulic fluids. In vacuum systems, pipe manifolds ensure that negative pressure is evenly distributed to multiple points.
Elbows and angle fittings
Elbows and angle fittings can be used to change the direction of the pipe, e.g. to avoid obstacles such as walls, etc. They are typically available with 45 and 90 degree angles, but also with 60 degree angles for special requirements. Elbows and angle fittings are also used to fabricate space-conserving pipe systems.
Elbows and angle fittings are available in all systems with different shapes (usually male or female), connectors and angles. They are often also available with the option to change cross-sections by reduction.
T-fittings and cross fittings
T-fittings and cross-fittings allow the medium to be distributed to several branches, e.g. in networks with several connected loads. T-fittings or cross-fittings can be used to create branches in further lines. Cross fittings are ideal for complex systems, especially when space needs to be conserved.
T-fittings and cross-fittings are also available in all systems with different shapes (male or female), connectors and angles. There is also the option to change the cross-section by reduction.
Reductions/reducers
Reducers connect pipes of different diameters. Reducers are often used to change flow rates of a medium within a system. Common ways to change the cross section of a line are reduction rings and eccentric or concentric reducers. Reducers are specified by the direction of flow, e.g. from inlet to outlet. For example, 1/4" to 3/4" means: Inlet with a 1/4 inch (approx. 6 mm) connector and outlet with a 3/4 inch (approx. 19 mm) connector. The specification also states whether the adapter has an internal or external thread.
Caps and Plugs
Caps and plugs permanently or temporarily close pipe ends securely, e.g. when a line is no longer operated. The closure prevents overflow or pressure loss. They may also be used temporarily during pipe system maintenance or pressure testing.
Optimizing pipe connections
There are a few things to keep in mind to ensure that the pipe connection is secure.
Preliminary considerations for pipe connections
There are a few things to consider in order to find the right connector from among the many options. When connecting pipes, problems often occur, for example when two different materials are connected together. Some material combinations react with each other and create a higher risk of corrosion. Even an incorrectly selected pipe connector or excessive force during assembly are common causes of a faulty connection.
The most important points to clarify in advance are therefore:
- Intended use and medium (hydraulic, pneumatic, vacuum, liquid, gas)
- releasable / non-releasable
- Possible chemical reaction of the connector and pipe system materials (non-noble and noble material)
- Temperature
- Is the connector rated for the pressure and medium?
- Are there any regulations to follow (food compatibility, etc.)?
- What is the flow direction? What options and flow direction for manifolds?
- What outlets are required on manifolds (inside/outside and cross-section)?
- Selection of the then still possible system and options for assembly (screws, soldering, flanges, press fits, etc.)
- What tools are needed? Common examples include pipe cutters, pipe wrenches, standard wrenches and a bubble level.
Connection options by pipe material
Different types of pipe connections are available depending on the material and the insert:
- Steel pipes: Preferably connected by welding, otherwise e.g. with flange connections or screw connections (e.g. threaded fittings).
- Copper pipes: Preferably soldering or pressing. Press fittings are for example frequently used in heating applications.
- Plastic pipes: Preferably plug-in connections, clamping connections, also adhesive-bonding and welding. For plug-in connections, the pipe is for example simply inserted into a fitting. Additional tools are not required.
- Stainless steel pipes: Preferably pressing, welding. Press fittings are also a quick and clean method.
- Composite pipes: Preferably pressing or clamping. Clamp fittings secure the pipe with a cap nut.
- Cast pipes: Preferably flanges, socket union. Socket unions have a sealing ring installed, which ensures a particularly tight connection.
Suitable Materials by Application
Choosing the right material depends on the desired application. For example, high corrosion resistance of the pipe connection is essential if water flows permanently through a pipe. Conversely, if high pressure prevails in the pipe, this should also be taken into account when selecting the pipe connection. The following overview outlines some common materials and their application:
- PVC: Suited for water systems because they are resistant to chemicals and corrosion.
- Copper: Copper is lightweight and malleable with relatively good corrosion resistance.
- Brass: In addition to corrosion resistance, brass has a high compressive load capacity.
- Stainless steel: Stainless steel is particularly robust and durable.
- Black steel (carbon steel): low cost, high compressive strength and temperature resistance, but low corrosion resistance
- Galvanized steel: slightly higher cost than black steel, but offers improved corrosion resistance and compatibility with other pipe materials while having approximately the same properties
We recommend our Steel Materials Guide to optimize your choice of steel material.
Cutting and joining pipes
There are straight pipes in standard lengths of e.g. two, three or six meters. For complicated pipe runs, it is therefore often necessary to shorten the pipes to the required length. Pipes with unprepared ends are also sometimes sold, i.e. they are not deburred on the cutting edges. In order to optimize the fit of the pipe connection, it is therefore essential to observe certain things in advance during processing, e.g. when cutting and deburring pipes.
Using a pipe cutter, many metal pipes and plastic pipes can be cut accurately and straight without crushing the pipe. The pipe is then deburred. Especially metal pipes such as copper pipes should be deburred to prevent damaging the fittings, which creates a risk of leakage. But deburring PVC pipes is also recommended. Deburring pipes contributes significantly to the quality and longevity of pipe connections and the entire pipe system. The deburring tool removes sharp edges and burrs. They are available in hand-operated and automatic versions.
Once the pipes are prepared properly, the pipe fitting can be seated. It is important to ensure a tight fit. However, the pipe fitting should not be threaded on excessively tights as this may cause over-threading. Finally, the pipe connection should be checked for leaks. This can be done, e.g., by allowing the medium to flow in. It is of course better to detect leaks beforehand, e.g. with a leak test device or a special leak spray. The leak spray is used to apply a foam or soapy liquid, which then makes bubbles at the leak.
Standardization: Various standards for pipe fittings
Pipe fittings are classified by common threading standards.
The following table summarizes the most important ones:
| Thread Standard | Specific standards | Description |
|---|---|---|
| NPT (national pipe thread) | ANSI/ASME B1.20.1 | NPT is a US standard for tapered threads, which are mainly used in the USA. It provides a tight joint by tapering the threads. |
| SAE (Society of Automotive Engineers) | SAE J514, SAE J1453 (Hydraulic fittings) | SAE threads and fittings are commonly used in the automotive and mechanical engineering industries. They include flared and O-ring joints for hydraulic applications. |
| BSP (British Standard Pipe) | BS EN 10226, BS 21, ISO 7/1 | BSP is a standard for cylindrical (BSPP) and conical (BSPT) threads that are mainly used in Europe and the Commonwealth. BSPP stands for "British Standard Pipe Parallel," whereas BSPT stands for "British Standard Pipe Tapered". |
| BSPT (British Standard Pipe Tapered) | ISO 7/1, BS EN 10226-1 | BSPT threads are conical and thus make a tight joint. They are often used in high pressure applications. |
| DIN (German Institute for Standardization) | DIN 2353, DIN ISO 8434-1 | DIN threads are mainly used in Europe and are intended for hydraulic and pneumatic systems. They provide secure and leak-free joints. |
| JIC (Joint Industry Council) | SAE J514 | JIC (also known as 37-degree flare fittings) are hydraulic pipe fittings that are widely used in the mechanical engineering and agricultural industry. |
| ISO (International Organization for Standardization) | ISO 8434, ISO 49 | ISO standards cover a variety of pipe fittings and support international compatibility and safety. |
Please visit our extensive techblog for more information on standard pipe thread dimensions.