PARTING LOCK SETS
Features
2.Enables accurate mold opening movement with no reaction.
3.Can also be used for low-pressure molding as it imposes little load when locking.
4.Functions regardless of the order of mold closing processes.
5.Makes the slide lock retreat if the runner stripper side closes before the parting line.
| No. | H |
|---|---|
| PLS | 50 |
| PLM | 68 |
| PLL | 86 |

(Fig. 2) Mold opened

| No. | S*(mm) |
|---|---|
| PLS | Approx.2 |
| PLM | Approx.11 |
| PLL | Approx.15 |
(Fig. 3) Release point of the cam lock
The release point is where the release
bar's end comes above the Smm *cam
holder's top surface.
*Use the S values shown in the table as
reference only. Make sure to check the
actual release timing on the site.

(Fig.4) Parting Line is released
Notes
1.Always use more than two sets on a mold.2.Use this parting lock set within the following load limits:
PLS/PLSW ton or less per mold(when 2 sets are used)
PLM1.8 tons or less per mold(when 2 sets are used)
PLL4 tons or less per mold(when 2 sets are used)
3.Maintain proper alignment of the right and left release points to avoid uneven contact and resultant breakage.